AbstractionManager Class |
Provides method for creating builder for abstraction commands in a fem part
|
AdaptivityExclusionZone Class |
Represents a NXOpen.CAE.AdaptivityExclusionZone . |
AdaptivityExclusionZoneBuilder Class |
Builds a NXOpen.CAE.AdaptivityExclusionZone object which represets adaptivity meta solution related exclusion zones. |
AdaptivityExclusionZoneCollection Class |
Represents a collection of correl meta solution. |
AdaptivityMetaSolution Class |
Represents a NXOpen.CAE.AdaptivityMetaSolution . |
AdaptivityMetaSolutionBuilder Class |
Builds a NXOpen.CAE.AdaptivityMetaSolution object which represets a recipe for generating adaptive remesh. |
AdaptivityMetaSolutionCollection Class |
Represents a collection of adaptivity meta solution. |
AdjacentFaceMethod Class |
Represents the output from the adjacent face smart selector method |
AfuAbscissaHeaderInfo Class |
Represents the data to define abscissa header information for an afu record
|
AfuData Class |
the data used to create an AFU Data Record |
AfuDataConvertor Class |
Convert data values for the AFU Data Record |
AfuHeaderId Class |
the data used to create header id information for an AFU Data Record |
AfuManager Class |
AFU File and Data Record Manager |
AfuMathFastRMSInfo Class |
Represents the Fast RMS parameter information
|
AfuMathFastRMSOutput Class |
Represents the Fast RMS output information
|
AfuMathOperation Class |
Does math operations on the AFU Data Records |
AfuOrdinateHeaderInfo Class |
Represents the ordinate header information for an afu record
|
AfuZHeaderInfo Class |
Represents the Z axis header information for an afu record
|
AssignNodalCSBuilder Class |
Represents a NXOpen.CAE.AssignNodalCSBuilder |
AssociationUtilities Class |
Represents Physical NXOpen.CAE.AssociationUtilities class |
AssyFEModel Class |
This class represents an Assembly Finite Element Model. This class will act as the gateway to the Finite Element Nodes ( NXOpen.CAE.FENode ) and Elements ( NXOpen.CAE.FEElement ) in the model. Only one instance of this class will exist in each assyfem part file
|
AssyFemPart Class |
Represents an NX part of type .afm.
|
AttachElementsBuilder Class |
Represents a NXOpen.CAE.AttachElementsBuilder |
AutoBCBuilder Class |
Builds one or more NXOpen.CAE.SimSimulationObject object(s). |
AutoCyclicSymmetryPairsBuilder Class |
Builds a NXOpen.CAE.AutoPairs object which represents a recipe for generating face pairs from a selected set of faces in the model. |
AutoMacViewerBuilder Class |
Represents the correlation pairing viewer builder |
AutoPairs Class |
Represents an autopairs obj
|
AutoPairsBuilder Class |
Builds a NXOpen.CAE.AutoPairs object which represets a recipe for generating face pairs from a selected set of faces or solids in the model whose distance is less than a specified tolerance. |
AutomaticMorphBuilder Class |
Represents a NXOpen.CAE.AutomaticMorphBuilder |
AutomaticSweepBetweenSelection Class |
Builder for creating Manual Hex Mesh - Face Dependency type - Multi Face Automatic |
AxiSymmetricParameters Class |
Implementation of axi-symmetry utility |
BCSelectionDisplayBuilder Class |
This class provides BC Selection Visual Display support, use this class to get the BC types in current solution, adds special BCs to list, and display the BC’s selection geometry with the BC’s color to do visually check |
BaseFEModel Class |
This class represents an Assembly Finite Element Model. This class will act as the gateway to the Finite Element Nodes ( NXOpen.CAE.FENode ) and Elements ( NXOpen.CAE.FEElement ) in the model. Only one instance of this class will exist in each assyfem part file
|
BaseFemPart Class |
Represents an NX part of type .afm.
|
BaseIteration Class |
This class provides interfaces to query iteration attributes |
BaseLoadcase Class |
This class provides interfaces to query loadcase attributes |
BaseResultType Class |
This class provides interfaces to query result type attributes |
BcLabelManagerBuilder Class |
Represents a NXOpen.CAE.BcLabelManagerBuilder builder which can be used to renumber NXOpen.CAE.SimBC id. |
BeamEADBuilder Class |
This class provides Beam/Bar Associated Data Support |
BeamElementInfo Class |
Represents a Beam Element Information. |
BeamElementInfoHandler Class |
Represents a Beam Element Information Hanlder. |
BeamSection Class |
Represents a Beam Cross Section |
BeamSectionCollection Class |
|
BeamSectionOffsetOptions Class |
|
BeamSectionOptions Class |
Represents the synchronize options to be used when a FEM part is created These options will be used to synchronize the specified entities from the master CAD part file to the FEM part file
|
BeamSectionOrientationOptions Class |
|
Bolt Class |
Represents Bolt |
BoltBuilder Class |
Represents a NXOpen.CAE.BoltBuilder |
BoltCollection Class |
Provides method for creating builder for bolt operation commands in a fem/afem part
|
BoundingVolume Class |
Represents a NXOpen.CAE.BoundingVolume . |
BoundingVolumeBuilder Class |
Represents a CAE.BoundingVolume builder |
BoundingVolumeCollection Class |
Represents a collection of bounding volumes. |
BushingEADBuilder Class |
This class provides Bushing Associated Data Support |
CADModeling Class |
The CADModeling class provides method to create cad face using polygon face |
CAEBody Class |
Represents a CAE body geometry
|
CAEConnection Class |
Represents Connection Recipe |
CAEConnectionBuilder Class |
Builder for creating Connection Recipes |
CAEConnectionCollection Class |
Provides method for creating builder for connection operation commands in a fem/afem part
|
CAEEdge Class |
Represents a CAE edge geometry
|
CAEFace Class |
Represents a CAE face geometry
|
CAESet Class |
Represents a group of CAE object sets. The objects in each set can be used to create loads, constraints ..etc
|
CAEVertex Class |
Represents a CAE vertex geometry
|
CAEWeldConnection Class |
Represents WeldConnection Recipe |
CAEWeldConnectionBuilder Class |
Builder for creating 1D Weld Connection |
CaeDOFSet Class |
Represents a dofset class NXOpen.CAE.CaeDOFSet . |
CaeDOFSetCollection Class |
|
CaeDOFSetDisplay Class |
Represents a DOF Set display attributes
|
CaeDataContainer Class |
Represents a list of named properties, where the property name is a unique string. |
CaeGroup Class |
Represents a group class NXOpen.CAE.CaeGroup . |
CaeGroupCollection Class |
|
CaePart Class |
This is an abstract class for NX parts of type .fem and .sim
|
CaeRegion Class |
Represents a cae region object. |
CaeRegionBuilder Class |
Represents a NXOpen.CAE.CaeRegionBuilder builder |
CaeRegionCollection Class |
Provides methods for managing CAE.CaeRegion in a sim part
|
CaeSession Class |
This class provides access to all session related CAE functionality
|
CfdAutoRefinementConstraint Class |
The automatic refinement constraint is used by surface wrap recipes |
CfdAutoRefinementConstraintBuilder Class |
Represents a NXOpen.CAE.CfdAutoRefinementConstraint builder |
CfdAutoRefinementConstraintCollection Class |
Provides methods for managing automatic refinement constraints:py:class:CAE.CfdAutoRefinementConstraint in a fem part
|
CfdContactPreventionConstraint Class |
The contact prevention constraint is a type of constraint which is used by the Fluid Domain Recipe to generate a fluid domain. |
CfdContactPreventionConstraintBuilder Class |
Represents a NXOpen.CAE.CfdContactPreventionConstraint builder |
CfdContactPreventionConstraintCollection Class |
Provides methods for managing Contact Prevention Constraints:py:class:CAE.CfdContactPreventionConstraint in a fem part
|
CfdLocalResolutionConstraint Class |
The local resolution constraint is a type of constraint which is used by the Fluid Domain Recipe to generate a fluid domain. |
CfdLocalResolutionConstraintBuilder Class |
Represents a NXOpen.CAE.CfdLocalResolutionConstraint builder |
CfdLocalResolutionConstraintCollection Class |
Provides methods for managing Local Resolution Constraints:py:class:CAE.CfdLocalResolutionConstraint in a fem part
|
CircularEdgeMethod Class |
Represents the output from the circular edge smart selector method |
CircularImprintBuilder Class |
Builder for creating Circular Imprint |
ClippingParameters Class |
This class is worked as a packet of information that can be used to set the clipping parameters of a NXOpen.CAE.Post object. |
ComacViewerBuilder Class |
Represents the correlation MAC matrix viewer builder |
CombineTrisBuilder Class |
Builder for creating Combine Tris |
CompanionResult Class |
Represents additional results data that will augment a primary set of Analysis results associated to a NXOpen.CAE.SimSolution .
|
CompanionResultBuilder Class |
Represents a NXOpen.CAE.CompanionResult builder and can be used to create or edit an NXOpen.CAE.CompanionResult |
CompanionResultCollection Class |
|
ConflictResolutionBuilder Class |
Represents a NXOpen.CAE.ConflictResolutionBuilder builder which can resolve conflicts between the two input BCs by a specified rule |
ConstraintResolutionBuilder Class |
Represents a NXOpen.CAE.ConstraintResolutionBuilder builder which can resolve conflicts between the two input constraints by a specified rule |
ContactMeshBuilder Class |
Represents a NXOpen.CAE.ContactMeshBuilder |
ConvexMeshBuilder Class |
Represents a NXOpen.CAE.ConvexMeshBuilder |
CorrelAlignmentBuilder Class |
This builder is used to control the alignment parameters of a NXOpen.CAE.CorrelSolution |
CorrelApplyAlignmentFromBuilder Class |
This builder is used to apply the alignment matrix read from selected xml file to the test model |
CorrelBaseBuilder Class |
Represents the abstract builder class for all objects defined in correl meta solution |
CorrelFineTuneAlignmentBuilder Class |
This builder is used to nudge the alignment by a fine adjustment |
CorrelManager Class |
Represents the correl manager that contains all correl and pre-test objects |
CorrelModePairingBuilder Class |
This builder is used to control the mode pairing behavior of a NXOpen.CAE.CorrelSolution |
CorrelSolution Class |
Represents a NXOpen.CAE.CorrelSolution , which is a meta-solution used to compare results from two structural dynamics solutions |
CorrelSolutionBuilder Class |
This is a manager to the CAE.CorrelSolution class. |
CorrelSolutionCollection Class |
Represents a collection of correl meta solution |
CreateJtBuilder Class |
Represents a NXOpen.CAE.CreateJtBuilder |
CrossSectionParameters Class |
This class is worked as a packet of information that can be used to change cross-section state. |
CyclicSymmetricParameters Class |
Implementation of axi-symmetry utility |
CylinderFaceMethod Class |
Represents the output from the cylinder face smart selector method |
DeformationParameters Class |
This class is worked as a packet of information that can be be used to deform NXOpen.CAE.Post objects. |
DeletePolygonFaceBuilder Class |
Builder for Delete Polygon Face |
DependentMesh Class |
Represents Mesh Recipe |
DependentMeshBuilder Class |
Represents a NXOpen.CAE.Mesh2d |
DependentMeshListItemBuilder Class |
Represents a NXOpen.CAE.DependentMeshListItemBuilder |
DependentMeshListItemBuilderList Class |
Represents a list of objects. |
DestinationCollectorBuilder Class |
Represents a Element Collector Container (Ecc) selection |
DurabilityAxisSearch Class |
Represents a NXOpen.CAE.DurabilityAxisSearch . |
DurabilityAxisSearchCollection Class |
Represents a collection of stress axes. |
DurabilityDamageEvaluationBuilder Class |
Represents the builder for evaluating durability damage. |
DurabilityDataControlBuilder Class |
Represents a builder class for the transient event data control. |
DurabilityEvaluateFatigueHistoryBuilder Class |
Represents the builder for evaluating fatigue histories. |
DurabilityEvent Class |
Represents a NXOpen.CAE.DurabilityEvent , which is an event of a durability solution process. |
DurabilityEventBuilder Class |
Represents the abstract builder class for all durability events. |
DurabilityEventCollection Class |
Represents a collection of durability events. |
DurabilityEventFatigueSettingsBuilder Class |
Represents a builder class for the event fatigue settings. |
DurabilityEventOverridesBuilder Class |
Represents a builder class for Event Overrides. |
DurabilityEventSolverBuilder Class |
Represents the builder for solving the durability event. |
DurabilityEventStrengthSettingsBuilder Class |
Represents a builder class for the event strength settings. |
DurabilityExcitation Class |
Represents a NXOpen.CAE.DurabilityExcitation . |
DurabilityExcitationBuilder Class |
Represents the abstract builder class for all durability excitations. |
DurabilityExcitationCollection Class |
Represents a collection of durability excitations. |
DurabilityFatigue Class |
Represents a NXOpen.CAE.DurabilityFatigue . |
DurabilityFatigueCollection Class |
Represents a collection of event fatigue settings. |
DurabilityFunctionExcitation Class |
Represents a NXOpen.CAE.DurabilityFunctionExcitation . |
DurabilityFunctionExcitationBuilder Class |
Represents a NXOpen.CAE.DurabilityFunctionExcitation builder. |
DurabilityLoadPattern Class |
Represents a NXOpen.CAE.DurabilityLoadPattern . |
DurabilityLoadPatternBuilder Class |
Represents a CAE.DurabilityLoadPattern builder. |
DurabilityManager Class |
Represents the durability manager that contains all durability objects. |
DurabilityMetaSolution Class |
Represents a NXOpen.CAE.DurabilityMetaSolution . |
DurabilityMetaSolutionBuilder Class |
Represents a NXOpen.CAE.DurabilityMetaSolution builder. |
DurabilityMetaSolutionCollection Class |
Represents a collection of correl meta solution. |
DurabilityRandomEvent Class |
Represents a NXOpen.CAE.DurabilityRandomEvent . |
DurabilityRandomEventBuilder Class |
Represents the builder for the random durability event. |
DurabilityRandomFatigue Class |
Represents a NXOpen.CAE.DurabilityRandomFatigue . |
DurabilityRandomFatigueBuilder Class |
Represents a builder class for the event fatigue settings. |
DurabilityRandomFatigueCollection Class |
Represents a collection of random fatigue. |
DurabilityResultPath Class |
Represents a NXOpen.CAE.DurabilityResultPath . |
DurabilityResultPathBuilder Class |
Represents a NXOpen.CAE.DurabilityResultPath builder. |
DurabilityResultsReportBuilder Class |
Represents the builder for reporting the durability results. |
DurabilitySolveOptions Class |
Represents a NXOpen.CAE.DurabilitySolveOptions . |
DurabilitySolveOptionsCollection Class |
Represents a collection of correl meta solution. |
DurabilitySolverBuilder Class |
Represents the builder for solving the durability solution process. |
DurabilityStaticEvent Class |
Represents a NXOpen.CAE.DurabilityStaticEvent . |
DurabilityStaticEventBuilder Class |
Represents the builder for the static durability event. |
DurabilityStrainGageAnalyzerBuilder Class |
Represents the builder for analyzing strain gage data. |
DurabilityStrength Class |
Represents a NXOpen.CAE.DurabilityStrength . |
DurabilityStrengthCollection Class |
Represents a collection of event strength settings. |
DurabilityStressAxesBuilder Class |
Represents a builder class for the event fatigue settings. |
DurabilityTransientEvent Class |
Represents a NXOpen.CAE.DurabilityTransientEvent . |
DurabilityTransientEventBuilder Class |
Represents the builder for the transient durability event. |
EdgeDensity Class |
Represents a CAE edge density
|
EdgeFaceImprintBuilder Class |
Builder for creating Face Face Imprint |
EdgePathMethod Class |
Represents a NXOpen.CAE.EdgePathMethod . |
EdgeSticherBuilder Class |
Represents a NXOpen.CAE.EdgeSticherBuilder |
ElemEdgePathMethod Class |
Represents a NXOpen.CAE.ElemEdgePathMethod . |
ElemLabelMethod Class |
Represents the output from the elem label smart selector method |
ElementConnectivityBuilder Class |
Represents a NXOpen.CAE.ElementConnectivityBuilder |
ElementCreateBuilder Class |
Represents a NXOpen.CAE.ElementCreateBuilder which allows you to manually create elements from existing nodes. |
ElementDeleteBuilder Class |
Represents a NXOpen.CAE.ElementDeleteBuilder |
ElementDetachBuilder Class |
Represents a NXOpen.CAE.ElementDetachBuilder |
ElementExtractBuilder Class |
Builder for creating Element Extract |
ElementExtrudeBuilder Class |
Represents a NXOpen.CAE.ElementExtrudeBuilder |
ElementInfoUtils Class |
Represents a system to query information about FE-based elements |
ElementModifyLabelBuilder Class |
Represents a NXOpen.CAE.ElementModifyLabelBuilder |
ElementModifyOrderBuilder Class |
Represents a NXOpen.CAE.ElementModifyOrderBuilder |
ElementModifyTypeBuilder Class |
Represents a NXOpen.CAE.ElementModifyTypeBuilder |
ElementProjectBuilder Class |
Represents a NXOpen.CAE.ElementProjectBuilder |
ElementReflectBuilder Class |
Represents a NXOpen.CAE.ElementReflectBuilder |
ElementRevolveBuilder Class |
Represents a NXOpen.CAE.ElementRevolveBuilder |
ElementSplitBuilder Class |
Represents a NXOpen.CAE.ElementSplitBuilder |
ElementTranslateBuilder Class |
Represents a NXOpen.CAE.ElementTranslateBuilder |
ElementTypeBuilder Class |
Represents the specification of the FEA Element Type for a meshing dialog. |
ElementTypes Class |
Represents an NXOpen.CAE.ElementTypes class. |
FEElemEdge Class |
Represents a Finite Element Edge which can be shared by more that one element. |
FEElemFace Class |
Represents a Finite Element Face. |
FEElement Class |
Represents a Finite Element. |
FEElementLabelMap Class |
Represents a Elementl Label to an CAE.FEElement map, it can be used to quickly convert a CAE.FEElement label, which is generally used in solver input files and results files, in the element object itself CAE.FEElement
|
FEModel Class |
This class represents a Finite Element Model. This class will act as the gateway to the Finite Element Nodes (CAE.FENode ) and Elements (CAE.FEElement ) in the model. Only one instance of this class will exist in each fem part file
|
FEModelOccAttribute Class |
This class represents an Interface to the Finite Element Model Attributes.
|
FEModelOccurrence Class |
This class represents a Finite Element Model Occurrence. Only one instance of this class will exist in each sim part file
|
FENode Class |
Represents a Finite Element Node. |
FENodeLabelMap Class |
Represents a Nodel Label to an CAE.FENode map, it can be used to quickly convert a CAE.FENode label, which is generally used in solver input files and results files, in the node object itself CAE.FENode
|
FaceDensity Class |
Represents a CAE face density
|
FaceFaceImprintBuilder Class |
Builder for creating Face Face Imprint |
FaceFromBoundaryBuilder Class |
Builder for creating Polygon Face by boundary |
FacetProximityBuilder Class |
Represents a CAE.FacetProximityBuilder builder |
FeatureEdgeNodeMethod Class |
Represents the output from the feature edge node smart selector method |
FeatureElemEdgeMethod Class |
Represents the output from the feature element edge smart selector method |
FeatureElemFaceMethod Class |
Represents the output from the feature element face smart selector method |
FeatureElemMethod Class |
Represents the output from the feature element smart selector method |
FeatureNodeMethod Class |
Represents the output from the feature node smart selector method |
FeatureShellElemMethod Class |
Represents the output from the feature shell element smart selector method |
FemCreationOptions Class |
Represents the FEM creation options to be used when a FEM part is created
|
FemPart Class |
Represents an NX part of type .fem.
|
FemSynchronizeOptions Class |
Represents the synchronize options to be used when a FEM part is created These options will be used to synchronize the specified entities from the master CAD part file to the FEM part file
|
FilletFaceMethod Class |
Represents the output from the fillet face smart selector method |
FlatPatternsBuilder Class |
Represents a Flat Patterns Builder. |
FluidDomainBuilder Class |
Represents a NXOpen.CAE.FluidDomainRecipe |
FluidDomainCollection Class |
Provides methods for managing fluid domains:py:class:NXOpen.CAE.FluidDomainRecipe in a fem part
|
FluidDomainRecipe Class |
Represents a FluidDomainRecipe
|
FreeBodyResultsBuilder Class |
Represents a NXOpen.CAE.FreeBodyResultsBuilder |
FreezeGeometryBuilder Class |
Builder for creating Freeze Geometry |
FreezeGeometryRecipe Class |
Represents FreezeGeometryRecipe |
Function Class |
Represents a function object |
FunctionBuilder Class |
This builder class is used to create or edit NXOpen.CAE.Function objects. |
FunctionCollection Class |
Represents a collection of function objects |
GRMSearch Class |
Contains methods for searching Teamcenter for CAE objects, as well as a cache of already found items.
|
GapEADBuilder Class |
This class provides Gap Associated Data Support |
GeneralGeometryBeamSection Class |
Represents a General Geometry Beam Cross Section |
GeneralGeometryBeamSectionBuilder Class |
Represents a NXOpen.CAE.GeneralGeometryBeamSectionBuilder |
GeometryRecipe Class |
Represents a Geometry Recipe
|
GeometryRecipeCollection Class |
|
GlobalLayupImportFromPptBuilder Class |
Represents a Global Layup IMport From Ppt Builder. |
GraphFromResultProbeBuilder Class |
Represents a NXOpen.CAE.GraphFromResultProbeBuilder |
GroupByBoundaryBuilder Class |
Represents a CAE.GroupByBoundaryBuilder .
|
GroupEdgeMethod Class |
Represents the output from the Group Edge smart selector method |
GroupElemEdgeMethod Class |
Represents the output from the Group Element Edge smart selector method |
GroupElemFaceMethod Class |
Represents the output from the Group Element Face smart selector method |
GroupElemMethod Class |
Represents the output from the Group Element smart selector method |
GroupElemMethodElemOption Class |
Represents the output from the Group Element smart selector method |
GroupFaceMethod Class |
Represents the output from the Group Face smart selector method |
GroupMethod Class |
Represents the output from the Group smart selector method |
GroupNodeMethod Class |
Represents the output from the Group Node smart selector method |
HoleElementEdgeMethod Class |
Represents the output from the hole element edge smart selector method |
HybridMesh Class |
Represents swept Mesh |
IAncillaryDisplayableEntity Class |
Represents an ANCILLARY_DISPLAYABLE_ENTITY. |
IBeamSectionBuilder Class |
Represents a NXOpen.CAE.IBeamSectionBuilder |
IExportableFEEntity Class |
Represents an EXPORTABLE_FE_ENTITY. |
IFEModel Class |
This class represents an Interface to the Finite Element Model.
|
IFolder Class |
This class represents an Interface to the Folder.
|
IHierarchicalFEModel Class |
This class represents an Interface to the Finite Element Model.
|
IMeshCollector Class |
Represents the base IMeshCollector class for MeshCollector and MeshCollectorOccurrence classes
|
IMeshManager Class |
Manages meshes:py:class:NXOpen.CAE.IMeshManager in cae parts
|
IPostScenarioDataSource Class |
This class represents a data source that can be used for a post processing scenario.
|
ImportSimulationBuilder Class |
Represents NXOpen.CAE.ImportSimulationBuilder |
ImportedResult Class |
Represents analysis results for a imported solver results file. |
ImportedSolutionBuilder Class |
Represents a NXOpen.CAE.ImportedSolutionBuilder builder |
ImprintBuilder Class |
Builder for creating Imprint |
InterpolationEADBuilder Class |
This class provides Interpolation Associated Data Support |
Iteration Class |
Represents iteration present in a NXOpen.CAE.Loadcase . |
Laminate Class |
|
LaminateDampingFactorBuilder Class |
The builder for the damping factor. |
LaminateDrapingData Class |
Encapsulate the ply information related to the draping algorithm |
LaminateDrapingDataBuilder Class |
Represents a NXOpen.CAE.LaminateDrapingData builder |
LaminateDrapingExtension Class |
Encapsulate the ply information related to a ply draping extension |
LaminateDrapingExtensionBuilder Class |
Builder class for NXOpen.CAE.LaminateDrapingExtension |
LaminateDrapingOrientation Class |
Encapsulates the ply draping results |
LaminateDynamicEvent Class |
The Laminate Dynamic Event. |
LaminateDynamicEventBuilder Class |
Represents a NXOpen.CAE.LaminateDynamicEvent builder |
LaminateDynamicEventCollection Class |
Represents a collection of laminate dynamic events |
LaminateDynamicSim Class |
The Laminate Dynamic Simulation builder is the journalling interface to build the LaminateDyanmicSim object. |
LaminateDynamicSimBuilder Class |
Represents a NXOpen.CAE.LaminateDynamicSim builder |
LaminateDynamicSimCollection Class |
Represents a collection of laminate dynamic sims |
LaminateElementFilterBuilder Class |
Represents a NXOpen.CAE.LaminateGraphicalReport builder |
LaminateExtrudeSetup Class |
Extrude Setup |
LaminateExtrudeSetupBuilder Class |
Represents a NXOpen.CAE.LaminateExtrudeSetup builder |
LaminateExtrudeSetupCollection Class |
Represents a collection of laminate extrusion setups |
LaminateFiberOrientationOptions Class |
Laminate Fiber Orientation Options |
LaminateFiberOrientationOptionsBuilder Class |
Represents a NXOpen.CAE.LaminateFiberOrientationOptions builder |
LaminateFillSetupBuilder Class |
Represents a NXOpen.CAE.LaminateFillSetupBuilder builder |
LaminateGlobalLayup Class |
Represent a global layup in the ply based modeling. |
LaminateGlobalLayupCollection Class |
|
LaminateGlobalLayupMgr Class |
Represent the laminate global layup manager which manages all the global layups in the laminate ply-based modeling project |
LaminateGlobalLayupPlyGroupCollection Class |
Represents a laminate layup in the global layup context (ply based modeling), which is defined by a sequence of NXOpen.CAE.LaminatePlyGroup , each with a name and a list of plies. |
LaminateGraphicalReport Class |
Represents a laminate graphical report |
LaminateGraphicalReportBuilder Class |
Represents a CAE.LaminateGraphicalReport builder |
LaminateGraphicalReportCollection Class |
Represents a collection of CAE.LaminateGraphicalReport |
LaminateIDrapingOrientation Class |
Encapsulates the ply draping results |
LaminateImportZonesBuilder Class |
Represents a NXOpen.CAE.LaminateImportZonesBuilder builder |
LaminateImportedLayupBuilder Class |
Represents a NXOpen.CAE.LaminateImportedLayupBuilder builder |
LaminateLayupOffset Class |
laminate layup offset
|
LaminateLayupOffsetBuilder Class |
Represents a NXOpen.CAE.LaminateLayupOffset builder |
LaminateLayupOffsetCollection Class |
Represents a collection of layup offset rules |
LaminateLockAngleBuilder Class |
Represents a builder |
LaminateManager Class |
Represents the laminate manager that contains all laminate post report setups |
LaminateMatOrientation Class |
Laminate Material Orientation |
LaminateMatOrientationBuilder Class |
Represents a NXOpen.CAE.LaminateMatOrientation builder |
LaminateMatOrientationCollection Class |
Represents a collection of layup growth rules |
LaminateModeProperty Class |
Represents the properties of one normal mode |
LaminateModePropertyCollection Class |
Represents a collection of laminate mode properties |
LaminatePly Class |
Represents one ply in a laminate layup
|
LaminatePlyCollection Class |
Represents a list of plies, which have a material, a thickness, an orientation, and a color
|
LaminatePlyFilterBuilder Class |
Represents a NXOpen.CAE.LaminatePlyFilterBuilder |
LaminatePlyGroup Class |
Represents one ply group in a laminate layup
|
LaminatePlyGroupCollection Class |
Represents a laminate layup, which is defined by a sequence of CAE.LaminatePlyGroup , each with a name and a list of plies
|
LaminatePlyMaxThicknessVarBuilder Class |
Builder used to modify the ply maximum accepted thickness variation for laminate fill |
LaminatePostReport Class |
Represents an advanced post reporting setup for laminate results. |
LaminatePostReportBuilder Class |
Represents a NXOpen.CAE.LaminatePostReport builder |
LaminatePostReportCollection Class |
Represents a collection of laminate post reports |
LaminateQuickReport Class |
Represents a laminate quick report |
LaminateQuickReportBuilder Class |
Represents a NXOpen.CAE.LaminateQuickReport builder |
LaminateQuickReportCollection Class |
Represents a collection of CAE.LaminateQuickReport |
LaminateRandomEvent Class |
The Laminate Dynamic Event. |
LaminateRandomEventBuilder Class |
Represents a NXOpen.CAE.LaminateRandomEvent builder |
LaminateRelabelPliesBuilder Class |
Represents a CAE.LaminateDynamicEvent builder |
LaminateSelectEntitiesBuilder Class |
Represents a NXOpen.CAE.LaminateSelectEntitiesBuilder |
LaminateSineEvent Class |
The Laminate Sine Event. |
LaminateSineEventBuilder Class |
Represents a NXOpen.CAE.LaminateSineEvent builder |
LaminateSpreadsheetReport Class |
Represents a laminate spreadsheet report |
LaminateSpreadsheetReportBuilder Class |
Represents a NXOpen.CAE.LaminateSpreadsheetReport builder |
LaminateSpreadsheetReportCollection Class |
Represents a collection of NXOpen.CAE.LaminateSpreadsheetReport |
LaminateViewDrapingResultsBuilder Class |
Represents the builder for the draping results viewer |
LayoutState Class |
This is the class representing a layout state.
|
LayoutStateApplicator Class |
|
LayoutStateBuilder Class |
|
LayoutStateCollection Class |
|
LayoutStateDataReference Class |
This class represents a data reference of a layout state.
|
LayoutStateDataReferenceCollection Class |
|
LbcAssociationMgr Class |
Represents an abstract NXOpen.CAE.LbcAssociationMgr |
Loadcase Class |
Represents loadcases present in a NXOpen.CAE.Result . |
LocalRemeshBuilder Class |
Represents a NXOpen.CAE.LocalRemeshBuilder |
LumpedMassEADBuilder Class |
This class provides LumpedMass Associated Data Support |
MMCCreateBuilder Class |
Represents a NXOpen.CAE.MMCCreateBuilder which can be used to create or edit NXOpen.CAE.MeshMate objects. |
ManualMorphBuilder Class |
Represents a NXOpen.CAE.ManualMorphBuilder |
ManualNodeAssociationBuilder Class |
Represents a NXOpen.CAE.ManualNodeAssociationBuilder |
ManualSweepBetweenListItemSelection Class |
Represents a NXOpen.CAE.ManualSweepBetweenListItemSelection |
ManualSweepBetweenListItemSelectionList Class |
Represents a list of objects. |
ManualSweepBetweenSelection Class |
Builder for creating Manual Hex Mesh - Face Dependency type. |
MappedHole Class |
Represents a CAE mapped hole
|
MappedMesh Class |
Represents Mesh Recipe |
MappedMeshBuilder Class |
Represents a Mapped Mesh Builder. |
MappedResult Class |
Represents analysis results for a imported solver results file. |
MaterialOptions Class |
Represents the material options to be used when assigning a material to cae part
|
MechanicalLoadSumBuilder Class |
Represents a NXOpen.CAE.MechanicalLoadSumBuilder |
MergeFaceBuilder Class |
Builder for creating Merge Face |
Mesh Class |
Represents a Mesh. |
Mesh0d Class |
Represents 0d Mesh |
Mesh0dBuilder Class |
Represents 0D Mesh * Used to create a NXOpen.CAE.Mesh0d |
Mesh1d Class |
Represents 1d Mesh |
Mesh1dBuilder Class |
Represents 1d Mesh * Used to create a NXOpen.CAE.Mesh1d |
Mesh2d Class |
Represents 2d Mesh |
Mesh2dBuilder Class |
Represents 2D Mesh * Used to create a NXOpen.CAE.Mesh2d |
Mesh2dFree Class |
Represents 2d Mesh |
Mesh3d Class |
Represents 3d Mesh |
Mesh3dHexBuilder Class |
Represents 3D Hex Mesh * Used to create a NXOpen.CAE.SweptMesh |
Mesh3dHybridBuilder Class |
Represents 3D Mesh * Used to create a CAE.Mesh3d |
Mesh3dTetBuilder Class |
Represents 3D Mesh * Used to create a CAE.Mesh3d |
MeshCollector Class |
Represents a MeshCollector. |
MeshCollectorBuilder Class |
Represents a NXOpen.CAE.MeshCollectorBuilder |
MeshCollectorDisplayDefaults Class |
Represents the base MeshCollectorDisplayDefaults class for Mesh, MeshCollector and MeshCollectorOccurrence classes
|
MeshCollectorDisplayDefaults0d Class |
Represents 0d Mesh Display Settings |
MeshCollectorDisplayDefaults1d Class |
Represents 1d Mesh Display Settings |
MeshCollectorDisplayDefaults2d Class |
Represents 2d Mesh Display Settings |
MeshCollectorDisplayDefaults3d Class |
Represents 3d Mesh Display Settings |
MeshCollectorOccurrence Class |
Represents a MeshCollector Occurrence
|
MeshCollectorOccurrenceBuilder Class |
Represents a NXOpen.CAE.MeshCollectorOccurrenceBuilder |
MeshControl Class |
Represents a MeshControl
|
MeshControlBuilder Class |
Represents a NXOpen.CAE.MeshControl |
MeshControlCollection Class |
Provides methods for managing mesh controls:py:class:NXOpen.CAE.MeshControl in a fem part
|
MeshControlDisplayManager Class |
Provides method for creating builder for mesh control display operation commands in both sim and fem part
|
MeshControlDisplayOptionsBuilder Class |
Represents a NXOpen.CAE.MeshControlDisplayOptionsBuilder |
MeshDisplaySettings Class |
Represents the base MeshDisplaySettings class for Mesh class
|
MeshDisplaySettings0d Class |
Represents 0d Mesh Display Settings |
MeshDisplaySettings1d Class |
Represents 1d Mesh Display Settings |
MeshDisplaySettings2d Class |
Represents 2d Mesh Display Settings |
MeshDisplaySettings3d Class |
Represents 3d Mesh Display Settings |
MeshFollower Class |
Represents Mesh Recipe |
MeshFromBoundaryBuilder Class |
Represents a NXOpen.CAE.MeshFromBoundaryBuilder |
MeshManager Class |
Creates Meshes:py:class:NXOpen.CAE.Mesh in a fem part
|
MeshManagerOccurrence Class |
Manages MeshOccurrencs and MeshCollectorOccurrences in a fem part
|
MeshManualSweepBetweenListItemSelection Class |
Represents a NXOpen.CAE.MeshManualSweepBetweenListItemSelection |
MeshManualSweepBetweenListItemSelectionList Class |
Represents a list of objects. |
MeshMate Class |
Represents a Mesh Mate
|
MeshPoint Class |
Represents a smart NXOpen.CAE.MeshPoint . |
MeshPointCollection Class |
|
MeshPointConicCenterBuilder Class |
Represents a NXOpen.CAE.MeshPointConicCenterBuilder |
MeshPointExistingPointBuilder Class |
Represents a NXOpen.CAE.MeshPointExistingPointBuilder |
MeshPointMultipleOnCurveBuilder Class |
Represents a NXOpen.CAE.MeshPointMultipleOnCurveBuilder |
MeshPointOnCurveBuilder Class |
Represents a NXOpen.CAE.MeshPointOnCurveBuilder |
MeshPointOnFaceBuilder Class |
Represents a NXOpen.CAE.MeshPointOnFaceBuilder |
MeshPointProjectBuilder Class |
Represents a NXOpen.CAE.MeshPointProjectBuilder |
MeshRefinementBuilder Class |
Represents Mesh Refinement * Used to create a NXOpen.CAE.MeshRefinementBuilder |
MeshShellFromSolid Class |
Represents 2d Mesh that follows 3d mesh |
ModelCheckManager Class |
Provides method for creating builder for node element operation commands in a fem part
|
ModelDisplayBuilder Class |
This class provides Model Display Data Support |
ModelUpdateCorrelMethodBuilder Class |
Represents a NXOpen.CAE.ModelUpdateCorrelMethodBuilder |
ModelUpdateDesignVariable Class |
Represents a NXOpen.CAE.ModelUpdateDesignVariable , which is a meta-solution used to update finite element models to match real life test data |
ModelUpdateDesignVariablesCollection Class |
Represents a collection of durability events. |
ModelUpdateDesignVariablesRapidCreateBuilder Class |
This class is the builder that is used for the rapid creation of design variables. |
ModelUpdateOptimOptionsBuilder Class |
Represents a NXOpen.CAE.ModelUpdateOptimOptionsBuilder |
ModelUpdateOptionsBuilder Class |
Represents a NXOpen.CAE.ModelUpdateOptionsBuilder |
ModelUpdateOverallWeightsBuilder Class |
Represents a NXOpen.CAE.ModelUpdateOverallWeightsBuilder |
ModelUpdateSensitivityViewerBuilder Class |
Represents NXOpen.CAE.ModelUpdateSensitivityViewerBuilder |
ModelUpdateSolution Class |
Represents a NXOpen.CAE.ModelUpdateSolution , which is a meta-solution used to update finite element models to match real life test data |
ModelUpdateSolutionBuilder Class |
Represents a NXOpen.CAE.ModelUpdateSolutionBuilder |
ModelUpdateSolutionCollection Class |
Represents a collection of model update meta solution |
ModelingObjectPropertyTable Class |
Represents a Modeling Object Property Table. |
ModelingObjectPropertyTableCollection Class |
Creates Modeling Object property tables:py:class:NXOpen.CAE.ModelingObjectPropertyTable in a fem model
|
ModifiableFEModelOccAttribute Class |
This class represents an Interface to the Finite Element Model.
|
MorphRevolvedMeshBuilder Class |
Represents a NXOpen.CAE.MorphRevolvedMeshBuilder |
MultipleElementCreateBuilder Class |
Represents a NXOpen.CAE.MultipleElementCreateBuilder which can be used to create mutiple elements in one efficient opertation. |
MultipleNodeCreateBuilder Class |
Represents a NXOpen.CAE.MultipleNodeCreateBuilder which can be used to create mutiple nodes in one efficient opertation. |
NamedPropTableWithTargetSet Class |
Represents a Solver Specific Modeling Object with associated target set(s)
|
NamedPropertyTable Class |
|
NodeAlignBuilder Class |
Represents a NXOpen.CAE.NodeAlignBuilder |
NodeAssociationBuilder Class |
Represents a NXOpen.CAE.NodeAssociationBuilder |
NodeCreateBuilder Class |
Represents a NXOpen.CAE.NodeCreateBuilder . |
NodeDeleteBuilder Class |
Represents a NXOpen.CAE.NodeDeleteBuilder |
NodeDissociationBuilder Class |
Represents a NXOpen.CAE.NodeDissociationBuilder |
NodeElementInfoBuilder Class |
Represents a NXOpen.CAE.NodeElementInfoBuilder |
NodeElementInfoManager Class |
Provides method for creating builder for node element info operation commands in both sim and fem part
|
NodeElementManager Class |
Provides method for creating builder for node element operation commands in a fem part
|
NodeLabelMethod Class |
Represents the output from the node label smart selector method |
NodeModifyLabelBuilder Class |
Represents a NXOpen.CAE.NodeModifyLabelBuilder |
NodeModifyLocationBuilder Class |
Represents a NXOpen.CAE.NodeModifyLocationBuilder |
NodeProjectBuilder Class |
Represents a NXOpen.CAE.NodeProjectBuilder |
NodeReflectBuilder Class |
Represents a NXOpen.CAE.NodeReflectBuilder |
NodeRotateBuilder Class |
Represents a NXOpen.CAE.NodeRotateBuilder |
NodeTranslateBuilder Class |
Represents a NXOpen.CAE.NodeTranslateBuilder |
NodesBetweenNodesBuilder Class |
Represents a NXOpen.CAE.NodesBetweenNodesBuilder |
NodesOnCurveBuilder Class |
Represents a NXOpen.CAE.NodesOnCurveBuilder |
NodesRepositionBuilder Class |
Represents a NXOpen.CAE.NodesRepositionBuilder |
NxBcPlotContours Class |
Represents a NXOpen.CAE.NxBcPlotContours object returned from NXOpen.CAE.SimBcPlotContoursBuilder.CreatePlotObject() in NXOpen.CAE.SimBcPlotContoursBuilder . |
OneDimensionalElementSplitBuilder Class |
Represents a NXOpen.CAE.OneDimensionalElementSplitBuilder |
OrderedEdgeElemMethod Class |
Represents the output from the ordered edge element smart selector method |
OrderedEdgeNodeMethod Class |
Represents the output from the ordered edge node smart selector method |
OrderedFeatureEdgeElemMethod Class |
Represents the output from the ordered feature edge element smart selector method |
OrderedFeatureEdgeNodeMethod Class |
Represents the output from the ordered feature edge node smart selector method |
OrderedSelection Class |
Represents list of ordered selection entitites |
PhysicalPropertyTable Class |
Represents a Physical Property Table. |
PhysicalPropertyTableCollection Class |
Creates physical property tables:py:class:NXOpen.CAE.PhysicalPropertyTable in a fem model
|
PolygonFaceOnMeshBuilder Class |
Builder for creating Polygon Face On Mesh |
PolygonGeometryManager Class |
|
Post Class |
Represents Post-Processing |
Post3DGraphBuilder Class |
Represents a NXOpen.CAE.Post3DGraphBuilder |
PostAnnotation Class |
Controls appearance of a annoation object in a postview. User must call CAE.PostAnnotation.Draw() to make changes visible.
|
PostAnnotationBuilder Class |
Builder to create NXOpen.CAE.PostAnnotation from NXOpen.CAE.Post <br/>User can pass entities which are same as current postview location. |
PostAnnotationPreference Class |
Represents Post-Annotation Preferences |
PostGraph Class |
This class provides interfaces to query graph attributes |
PostGraphAcrossIterationsBuilder Class |
Represents a NXOpen.CAE.PostGraphAcrossIterationsBuilder |
PostGraphAlongPathBuilder Class |
Represents a NXOpen.CAE.PostGraphAlongPathBuilder |
PostGraphBuilder Class |
Represents a NXOpen.CAE.PostGraphBuilder |
PostGraphOrbitBuilder Class |
Represents a NXOpen.CAE.PostGraphOrbitBuilder |
PostGraphPreference Class |
Represents Post-Graph Preferences |
PostIdentifyPreference Class |
Represents Post-Identify Preferences |
PostJtExportBuilder Class |
Represents a NXOpen.CAE.PostJtExportBuilder used for exporting JTs of Result Types in Post Processing |
PostLegendPreference Class |
Represents Post-Legend Preferences |
PostPreference Class |
Represents Post Preferences |
PostResultNavigatorPreference Class |
Represents Post-ResultNavigator Preferences |
PostResultPreference Class |
Represents Post-Result Preferences |
PostScenarioBuilder Class |
|
PostScenarioBuilderDataDefinitionCollection Class |
This is a collection of NXOpen.CAE.PostScenarioDataDefinition available to a NXOpen.CAE.PostScenarioBuilder for a selected Data Source |
PostScenarioConfigurationVariable Class |
A configuration variable to which values can be bound in order to define a user selection (NXOpen.CAE.PostScenarioSelectionParameters ) for a post scenario (NXOpen.CAE.PostScenarioBuilder ). |
PostScenarioConfigurationVariableCollection Class |
|
PostScenarioDataDefinition Class |
Represents a data source data definition.
|
PostScenarioDescriptor Class |
|
PostScenarioDescriptorCollection Class |
|
PostScenarioInputDefinition Class |
|
PostScenarioInputDefinitionCollection Class |
|
PostScenarioManager Class |
Manages the creation of a NXOpen.CAE.PostScenarioBuilder . |
PostScenarioParameters Class |
|
PostScenarioSelectionParameters Class |
The class handles the User Selection for a Scenario.
|
PostScenarioVariable Class |
|
PostScenarioVariableCollection Class |
|
PostScenarioVariant Class |
A dynamically typed scalar value.
|
PostScenarioVisualizationCollection Class |
Represents a collection of Visualizations available in a certain Scenario Definition’s Input Definition. |
PostScenarioVisualizationDefinition Class |
|
PreTestDofSet Class |
Represents Dof Set within a pre-test setup |
PreTestDofSetBuilder Class |
Represents a NXOpen.CAE.PreTestDofSet builder |
PreTestExciterConfig Class |
Represent a exciter selection configuration |
PreTestExciterConfigBuilder Class |
Represents a NXOpen.CAE.PreTestExciterConfig builder |
PreTestExciterConfigCollection Class |
Represents a collection of exciter selection configuration |
PreTestExciterSelectionControl Class |
Represents a pre-test exciter selection setup |
PreTestExciterSelectionDofSetCollection Class |
Represents a collection of exciter selection configuration. |
PreTestExportUnvBuilder Class |
This is a manager to the NXOpen.CAE.PreTestExportUnvBuilder class. |
PreTestSensorConfig Class |
Represent a sensor selection configuration |
PreTestSensorConfigBuilder Class |
Represents a NXOpen.CAE.PreTestSensorConfig builder |
PreTestSensorConfigCollection Class |
Represents a collection of sensor selection configuration |
PreTestSensorSelectionControl Class |
Represents a pre-test sensor selection setup |
PreTestSensorSelectionDofSetCollection Class |
Represents a collection of sensor selection configuration. |
PreTestSolution Class |
Represents a pre-test setup |
PreTestSolutionBuilder Class |
Represents a NXOpen.CAE.PreTestSolution builder |
PreTestSolutionCollection Class |
Represents a collection of pre-test setups |
PrimitiveMesh Class |
Represents Primitive Mesh |
PrimitiveMeshBuilder Class |
Represents Primitive Mesh * Used to create a CAE.Mesh |
PrimitiveRecipeMesh Class |
Represents a primitive recipe mesh. |
PrimitiveRecipeMeshBuilder Class |
Represents a Primitive Recipe Mesh * Used to create a CAE.Mesh |
ProjectNodesToCadGeometryBuilder Class |
Allows you to query the mesh nodes that are off the underlying Cad geometry by a given tolerance, and if requested this builder can adjust the node locations to put them back on to the underlying Cad geometry. |
PropertyTable Class |
Represents a property table
|
QueryCurve Class |
Represents a NXOpen.CAE.QueryCurve |
QueryCurveBuilder Class |
Represents a NXOpen.CAE.QueryCurveBuilder |
QueryCurveManager Class |
Provides methods for managing the query curves. |
QueryCurvePost Class |
Represents a NXOpen.CAE.QueryCurvePost Use NXOpen.CAE.ResultManager to create an instance of this class |
QueryCurveUsageOptions Class |
Represents the options to apply a query curve
|
ReassignElementsBuilder Class |
Represents a NXOpen.CAE.ReassignElementsBuilder |
RecipeSurfaceWrap Class |
Represents 2d mesh associated to fluid domain body, all from surface wrapper. |
RelatedElemEdgeMethod Class |
Represents the output from the related element edge smart selector method |
RelatedElemFaceMethod Class |
Represents the output from the related element face smart selector method |
RelatedElemMethod Class |
Represents the output from the related element smart selector method |
RelatedFaceMethod Class |
Represents the output from the related face smart selector method |
RelatedNodeMethod Class |
Represents the output from the related node smart selector method |
RemoveRibsBuilder Class |
Represents a NXOpen.CAE.RemoveRibsBuilder |
Result Class |
<para> This class provides interfaces to query analysis results. |
ResultAccess Class |
Represents a specific result state for a given NXOpen.CAE.Result . |
ResultManager Class |
Manages results |
ResultMeasure Class |
Represents a ResultMeasure class NXOpen.CAE.ResultMeasure . |
ResultMeasureCollection Class |
|
ResultMeasureModelSubset Class |
Represents a a subset of the model upon which to calculate results |
ResultMeasureModelSubsetFE Class |
Represents a FE-based subset of the model upon which to calculate results |
ResultMeasureModelSubsetGeom Class |
Represents a geometry-based subset of the model upon which to calculate results |
ResultMeasureResultAllOptions Class |
Represents the combination of all result options for result measure |
ResultMeasureResultDirectionOptions Class |
Represents the result directional options for result measure |
ResultMeasureResultDirectionSectionOptions Class |
Represents the result directional and beam/shell section options for result measure |
ResultMeasureResultOptions Class |
Represents the basic result options for result measure |
ResultMeasureResultSectionOptions Class |
Represents the result with beam/shell section options for result measure |
ResultParameters Class |
This class is worked as a packet of information that can be either be used to change result state or pass around for information exchange between two NXOpen.CAE.ResultAccess objects. |
ResultParametersWithProbe Class |
<para>To obtain an instance of this class use Session.ResultManager() . |
ResultProbe Class |
Result Probe Object.
|
ResultProbeBuilder Class |
Result probe Builder |
ResultType Class |
This class represents a result type from a result file. |
ResultVariable Class |
Controls Result Exp Object.
|
ResultsCombinationBuilder Class |
Represents a NXOpen.CAE.ResultsCombinationBuilder |
ResultsEnvelopeBuilder Class |
Represents a NXOpen.CAE.ResultsEnvelopeBuilder |
ResultsManipulationBuilder Class |
Represents an abstract NXOpen.CAE.ResultsManipulationBuilder |
ResultsModelExportBuilder Class |
Represents a NXOpen.CAE.ResultsModelExportBuilder |
ResultsReductionBuilder Class |
Represents a NXOpen.CAE.ResultsReductionBuilder |
SelectCAEBody Class |
Represents a single object selection. |
SelectCAEBodyList Class |
Represents a list of objects on a selection list. |
SelectCAEEdge Class |
Represents a single object selection. |
SelectCAEEdgeList Class |
Represents a list of objects on a selection list. |
SelectCAEFace Class |
Represents a single object selection. |
SelectCAEFaceList Class |
Represents a list of objects on a selection list. |
SelectElementsBuilder Class |
Represents a NXOpen.CAE.SelectElementsBuilder |
SelectElementsManager Class |
Provides method for creating builder for select element operation commands in both fem and sim part
|
SelectFEElemFaceList Class |
Represents a list of objects on a selection list. |
SelectFENode Class |
Represents a single object selection. |
SelectFENodeList Class |
Represents a list of objects on a selection list. |
SelectMeshList Class |
Represents a list of objects on a selection list. |
SetManager Class |
Represents a group of CAE object sets. The objects in each set can be used to create loads, constraints ..etc
|
ShapeMetricViewerBuilder Class |
Represents the correlation Shape metrics viewer builder |
Shell2SolidBuilder Class |
Represents 3D Tet Mesh * Used to create a CAE.Mesh3d |
ShellEADBuilder Class |
This class provides Shell Associated Data Support |
ShowAdjacentBuilder Class |
Represents a NXOpen.CAE.ShowAdjacentBuilder |
ShowAdjacentGroupMethod Class |
Represents the output from the Show Hide Group smart selector method |
ShowHideBuilder Class |
Represents a NXOpen.CAE.ShowHideBuilder |
ShowHideGroupMethod Class |
Represents the output from the Show Hide Group smart selector method |
ShowHideManager Class |
Provides method for creating builder for Show Hide operation commands in a fem/sim part
|
ShowOnlyBuilder Class |
Represents a NXOpen.CAE.ShowOnlyBuilder |
SimAutoBcRecipe Class |
Represents a simulation recipe containing the parameters needed for the generation of a set of face pairs from the faces/bodies in the model
|
SimBC Class |
|
SimBCBuilder Class |
This is a manager to the CAE.SimBC class. Objects of type CAE.SimBC can be created and edited only through this class
|
SimBCDisplay Class |
Represents a BC display attributes
|
SimBcGroup Class |
Represents a BC group in a solution or solution step
|
SimBcPlotContoursBuilder Class |
Represents a NXOpen.CAE.SimBcPlotContoursBuilder builder which can be used to generate a plot of a NXOpen.CAE.SimBC in the graphics area. |
SimBcXyPlotBuilder Class |
Represents a NXOpen.CAE.SimBcXyPlotBuilder builder which can be used to generate a XY plot of a NXOpen.CAE.SimBC in the graphics area. |
SimCondition Class |
|
SimConditionCollection Class |
|
SimConditionParam Class |
|
SimConditionParamCollection Class |
|
SimConditionSeqMgr Class |
This is the manager for Condition Sequences. Each Simulation has one manager.
|
SimConditionSequence Class |
|
SimConditionSequenceCollection Class |
|
SimConditionTimeStep Class |
|
SimConditionTimeStepCollection Class |
|
SimConstraint Class |
Represents a constraint
|
SimConstraintCollection Class |
|
SimConstraintGroup Class |
Represents a constraint group in a solution or solution step
|
SimConstraintSet Class |
Represents a cae constraint set object
|
SimConstraintSetBuilder Class |
Represents a CAE.SimConstraintSetBuilder builder |
SimConstraintSetCollection Class |
Provides methods for managing SimConstraintSet in a sim part
|
SimGroupContainer Class |
Represents UGS::CaeSim::LbcGroupContainer
|
SimLbcFolder Class |
Represents a folder object in the .sim files
|
SimLbcFolderCollection Class |
|
SimLoad Class |
Represents a load
|
SimLoadCollection Class |
|
SimLoadGroup Class |
Represents a load group in a solution or solution step
|
SimLoadRecipe Class |
This is the class handling the attributes of a load recipe.
|
SimLoadRecipeCollection Class |
|
SimLoadRecipeLbcGenerator Class |
|
SimLoadRecipeMapEntry Class |
|
SimLoadRecipeMapEntryCollection Class |
This class is a collection of :py:class: `NXOpen.CAE.SimLoadRecipeMapEntry`s.
|
SimLoadRecipeMapEntryTargetTypes Class |
The class handles the enum definitions needed by load recipe map entries
|
SimLoadRecipeMapping Class |
This is the class handling the mapping of a certain load type of a load recipe.
|
SimLoadRecipeMappingCollection Class |
This class is a collection of :py:class: `NXOpen.CAE.SimLoadRecipeMapping`s.
|
SimLoadRecipeSource Class |
This is the class handling the attributes of a source used by a load recipe.
|
SimLoadRecipeSourceCollection Class |
|
SimLoadRecipeTypes Class |
The class handles the enum definitions needed by load recipes
|
SimLoadSet Class |
Represents a cae load set object
|
SimLoadSetBuilder Class |
Represents a NXOpen.CAE.SimLoadSetBuilder builder |
SimLoadSetCollection Class |
|
SimMotionLoadsBuilder Class |
Represents a NXOpen.CAE.SimMotionLoadsBuilder |
SimMotionLoadsListItemBuilder Class |
Represents a NXOpen.CAE.SimMotionLoadsListItemBuilder |
SimPart Class |
Represents an NX part of type .sim.
|
SimRecipe Class |
This is an abstract class. for all simulation recipe classes
|
SimRecipeCollection Class |
|
SimResultReference Class |
Represents a Result Reference in the . |
SimSimulation Class |
This is the root object in a .sim file. Only one instance of this class will exist in each fem part file.
|
SimSimulationObject Class |
Represents a simulation object. |
SimSimulationObjectCollection Class |
|
SimSimulationObjectGroup Class |
Represents a simulation object group in a solution or solution step
|
SimSolution Class |
Represents a solution in the . |
SimSolutionCollection Class |
|
SimSolutionStep Class |
Represents a subcase/step in a solution. |
SimSolveManager Class |
|
SketchCurves Class |
Represents a Beam Cross Section |
SketchCurvesCollection Class |
|
SliverFaceMethod Class |
Represents the output from the sliver face smart selector method |
SmartSelectionManager Class |
Provides methods for creating smart selection methods in a cae part
|
SolidPropertyCheckBuilder Class |
Represents a NXOpen.CAE.SolidPropertyCheckBuilder |
SolutionManager Class |
Represents NXOpen.CAE.SolutionManager |
SolutionResult Class |
Represents analysis results for a given NXOpen.CAE.SimSolution . |
SolverAppendOption Class |
This class provides access to the append option setting for importing solver specific data into existing Fem/Sim
|
SpiderElementBuilder Class |
Represents a NXOpen.CAE.SpiderElementBuilder |
SpringEADBuilder Class |
This class provides Spring Associated Data Support |
StandardBeamSection Class |
Represents a Standard Beam Cross Section |
StandardBeamSectionBuilder Class |
Represents a NXOpen.CAE.StandardBeamSectionBuilder |
StepManager Class |
Represents NXOpen.CAE.StepManager |
SuppressHoleBuilder Class |
Builder for creating Hole Suppression Hole |
SurfaceCoatBuilder Class |
Builder for creating Surface Coat |
SweepBetweenMeshBuilder Class |
Builder for creating swept mesh between faces. |
SweptMesh Class |
Represents swept Mesh |
TangentContinuousEdgeMethod Class |
Represents the output from the circular edge smart selector method |
TangentFaceMethod Class |
Represents the output from the tangent face smart selector method |
ThickenMeshBuilder Class |
Represents a NXOpen.CAE.ThickenMeshBuilder |
ThicknessBuilder Class |
Represents a NXOpen.CAE.ThicknessBuilder |
ThicknessPlotContours Class |
Represents a NXOpen.CAE.ThicknessPlotContours object returned from NXOpen.CAE.ThicknessPlotContoursBuilder.CreatePlotObject() in NXOpen.CAE.ThicknessPlotContoursBuilder . |
ThicknessPlotContoursBuilder Class |
Represents a NXOpen.CAE.ThicknessPlotContoursBuilder builder which can be used to generate a plot of a NXOpen.CAE.SimBC in the graphics area. |
TransientResultsReductionBuilder Class |
Represents a NXOpen.CAE.TransientResultsReductionBuilder |
UnStitchEdgeBuilder Class |
Represents a NXOpen.CAE.UnStitchEdgeBuilder |
UserDefinedSolidBeamSection Class |
Represents a User-Defined Solid Beam Cross Section |
UserDefinedSolidBeamSectionBuilder Class |
Represents a NXOpen.CAE.UserDefinedSolidBeamSectionBuilder |
ViewLaminateBuilder Class |
Represents a View Laminate Builder. |
WeldBuilder Class |
Represents a NXOpen.CAE.WeldBuilder |
WeldRow Class |
Represents a CAE weld row
|