AfuDataConvertor Class

class NXOpen.CAE.AfuDataConvertor

Bases: object

Convert data values for the AFU Data Record

To obtain an instance of this class, refer to NXOpen.CAE.AfuManager

New in version NX5.0.0.

Methods

Method Description
GetFftComplexType Get the complex type of ordinate data by FFT @return Complex type of ordinate data after FFT
GetFftFrequencyData Get the values by Forward FFT.
GetFftTimeData Get the values by Inverse FFT.

Enumerations

AfuDataConvertorFft Enumeration Defines the way of FFT on AFU Data Record

Method Detail

GetFftComplexType

AfuDataConvertor.GetFftComplexType

Get the complex type of ordinate data by FFT

Signature GetFftComplexType(fftType, inComplexType)

Parameters:
Returns:

Complex type of ordinate data after FFT

Return type:

NXOpen.CAE.AfuDataOrdinateType

New in version NX5.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

GetFftFrequencyData

AfuDataConvertor.GetFftFrequencyData

Get the values by Forward FFT.

The input data should be Real data on Time domain and the output data will be Complex data on Frequency domain.

Signature GetFftFrequencyData(inXValues, inYValues)

Parameters:
  • inXValues (list of float) – X values of the input data
  • inYValues (list of float) – Y values of the input data
Returns:

a tuple

Return type:

A tuple consisting of (zValues, xValues, yValues). zValues is a list of float. Imaginary part of Y values of the output data xValues is a list of float. X values of the output data yValues is a list of float. Real part of Y values of the output data

New in version NX5.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

GetFftTimeData

AfuDataConvertor.GetFftTimeData

Get the values by Inverse FFT.

The input data should be Complex data on Frequency domain and the output data will be Real data on Time domain.

Signature GetFftTimeData(inXValues, inYValues, inZValues)

Parameters:
  • inXValues (list of float) – X values of the input data
  • inYValues (list of float) – Real part of Y values of the input data
  • inZValues (list of float) – Imaginary part of Y values of the input data
Returns:

a tuple

Return type:

A tuple consisting of (yValues, xValues). yValues is a list of float. Y values of the output data xValues is a list of float. X values of the output data

New in version NX5.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)