AfuManager Class¶
-
class
NXOpen.CAE.
AfuManager
¶ Bases:
object
AFU File and Data Record Manager
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX4.0.0.
“AfuDataConvertor”, ” Contains FFT operations for AFU data ” “AfuMathOperation”, ” Contains Math Operations for AFU data “
Methods¶
Method | Description |
---|---|
CopyRecords | Copy multiple AFU Data Records to an AFU file |
CreateAfuAbscissaHeaderInfo | Creates an afu abscissa header information data object @return Abscissa header information data NXOpen.CAE.AfuAbscissaHeaderInfo to be created |
CreateAfuData | Create an AFU Data Record object with specified axis definition @return AFU Data Record |
CreateAfuHeaderId | Create an AFU Header Id object @return AFU Header Id data |
CreateAfuOrdinateHeaderInfo | Creates an afu ordindate header information data object @return Ordindate header information data NXOpen.CAE.AfuOrdinateHeaderInfo to be created |
CreateAfuZHeaderInfo | Create an afu Z axis header information data object @return Z axis header information data NXOpen.CAE.AfuZHeaderInfo to be created |
CreateNewAfuFile | Create a new empty AFU file |
CreateRecord | Create a new AFU Data Record. |
DeleteAfuFile | Delete an AFU file |
DeleteRecords | Delete multiple AFU Data Records from an AFU file |
EditRecord | Edit an existing AFU Data Record. |
ExportAfu | Export an AFU Data Record to a CSV, MAT or DAC file |
ExportAfuFile | Export all Data Records of an AFU to a RPCIII file |
GetAfuData | Return data from an AFU Data Record @return Time stamp string indicates the last time the AFU Data Record was edited |
GetAfuUnitText | Return the unit text of AFU data like mm, sec etc. |
GetAfuUnitTypeText | Return the unit type text of AFU data like Displacement, Time etc. |
GetRecordIndexes | Return indices of all Data Records in an AFU file @return Index array of all Data Records in the AFU file. |
ImportAfu | Import AFU Data Records from a CSV, MAT, DAC or RPCIII file |
ListFileInformation | List header information of all AFU Data Records in an AFU file to listing window or a specified output file |
ListRecordInformation | List the AFU Data Record information to listing window or a specified output file |
RenameRecord | Rename an AFU Data Record |
Enumerations¶
AfuManagerWritingFileMode Enumeration | This enumeration defines the modes of outputting information to a file |
AfuDataConvertor¶
-
AfuManager.
AfuDataConvertor
¶ Contains FFT operations for AFU data
Signature
AfuDataConvertor()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.AfuDataConvertor
AfuMathOperation¶
-
AfuManager.
AfuMathOperation
¶ Contains Math Operations for AFU data
Signature
AfuMathOperation()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.AfuMathOperation
Method Detail¶
CopyRecords¶
-
AfuManager.
CopyRecords
¶ Copy multiple AFU Data Records to an AFU file
Signature
CopyRecords(sourceAfuFileNames, recordIndexes, destinationAfuFileName)
Parameters: - sourceAfuFileNames (list of str) – List of the AFU Files to be copied (full filenames)
- recordIndexes (list of int) – Indexes of the AFU Data Records to be copied. Each index Must begin with 1
- destinationAfuFileName (str) – Destination AFU file (full filename)
New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
CreateAfuAbscissaHeaderInfo¶
-
AfuManager.
CreateAfuAbscissaHeaderInfo
¶ Creates an afu abscissa header information data object
Signature
CreateAfuAbscissaHeaderInfo()
Returns: Abscissa header information data NXOpen.CAE.AfuAbscissaHeaderInfo
to be createdReturn type: NXOpen.CAE.AfuAbscissaHeaderInfo
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
CreateAfuData¶
-
AfuManager.
CreateAfuData
¶ Create an AFU Data Record object with specified axis definition
Signature
CreateAfuData(abscissaType)
Parameters: abscissaType ( NXOpen.CAE.AfuDataAbscissaType
) – Abscissa specific data typeReturns: AFU Data Record Return type: NXOpen.CAE.AfuData
New in version NX9.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
CreateAfuHeaderId¶
-
AfuManager.
CreateAfuHeaderId
¶ Create an AFU Header Id object
Signature
CreateAfuHeaderId()
Returns: AFU Header Id data Return type: NXOpen.CAE.AfuHeaderId
New in version NX5.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
CreateAfuOrdinateHeaderInfo¶
-
AfuManager.
CreateAfuOrdinateHeaderInfo
¶ Creates an afu ordindate header information data object
Signature
CreateAfuOrdinateHeaderInfo()
Returns: Ordindate header information data NXOpen.CAE.AfuOrdinateHeaderInfo
to be createdReturn type: NXOpen.CAE.AfuOrdinateHeaderInfo
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
CreateAfuZHeaderInfo¶
-
AfuManager.
CreateAfuZHeaderInfo
¶ Create an afu Z axis header information data object
Signature
CreateAfuZHeaderInfo()
Returns: Z axis header information data NXOpen.CAE.AfuZHeaderInfo
to be createdReturn type: NXOpen.CAE.AfuZHeaderInfo
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
CreateNewAfuFile¶
-
AfuManager.
CreateNewAfuFile
¶ Create a new empty AFU file
Signature
CreateNewAfuFile(afuFileName)
Parameters: afuFileName (str) – AFU filename New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
CreateRecord¶
-
AfuManager.
CreateRecord
¶ Overloaded method CreateRecord
CreateRecord(macroType, dataType, afuData)
CreateRecord(afuData)
-------------------------------------
Create a new AFU Data Record. Application type and usage type are specified to set the function data type of the AFU Data Record. Timestamp is outputted.
Signature
CreateRecord(macroType, dataType, afuData)
Parameters: - macroType (
NXOpen.CAE.XyFunctionMacroType
) – Application type of AFU Data Record used - dataType (
NXOpen.CAE.XyFunctionGeneralType
) – Usage type of AFU Data Record used - afuData (
NXOpen.CAE.AfuData
) – Afu data used to create AFU Data Record
Returns: Time stamp string indicates when the record was created
Return type: str
New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Create a new AFU Data Record. Application type and usage type are NOT specified. The function data type of the AFU Data Record will be set by
CAE.AfuData.FunctionDataType()
. Timestamp is NOT outputted.Signature
CreateRecord(afuData)
Parameters: afuData ( NXOpen.CAE.AfuData
) – Afu data used to create AFU Data RecordNew in version NX5.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
DeleteAfuFile¶
-
AfuManager.
DeleteAfuFile
¶ Delete an AFU file
Signature
DeleteAfuFile(afuFileName)
Parameters: afuFileName (str) – AFU filename New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
DeleteRecords¶
-
AfuManager.
DeleteRecords
¶ Delete multiple AFU Data Records from an AFU file
Signature
DeleteRecords(afuFileName, afuRecordIndexes)
Parameters: - afuFileName (str) – AFU file full name
- afuRecordIndexes (list of int) – List of Indexes of data records to be deleted from the AFU file. (Indexes begin with 1)
New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
EditRecord¶
-
AfuManager.
EditRecord
¶ Overloaded method EditRecord
EditRecord(macroType, dataType, afuRecordIndex, afuData)
EditRecord(afuRecordIndex, afuData)
-------------------------------------
Edit an existing AFU Data Record. Application type and usage type are specified to set the function data type of the AFU Data Record. Timestamp is outputted.
Signature
EditRecord(macroType, dataType, afuRecordIndex, afuData)
Parameters: - macroType (
NXOpen.CAE.XyFunctionMacroType
) – Application type of AFU Data Record used - dataType (
NXOpen.CAE.XyFunctionGeneralType
) – Usage type of AFU Data Record used - afuRecordIndex (int) – Index of the AFU Data Record in the AFU file. Must begin with 1
- afuData (
NXOpen.CAE.AfuData
) – Afu data used to create the AFU Data Record
Returns: Time stamp string indicates when the data record was last edited
Return type: str
New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Edit an existing AFU Data Record. Application type and usage type are NOT specified. The function data type of the AFU Data Record will be set by
CAE.AfuData.FunctionDataType()
. Timestamp is NOT outputted.Signature
EditRecord(afuRecordIndex, afuData)
Parameters: - afuRecordIndex (int) – Index of the AFU Data Record in the AFU file. Must begin with 1
- afuData (
NXOpen.CAE.AfuData
) – Afu data used to create the AFU Data Record
New in version NX5.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
ExportAfu¶
-
AfuManager.
ExportAfu
¶ Export an AFU Data Record to a CSV, MAT or DAC file
Signature
ExportAfu(afuFileName, recordIndex, exportFileName)
Parameters: - afuFileName (str) – AFU filename
- recordIndex (int) – Index of the AFU Data Record to be exported
- exportFileName (str) – Name of destination file to which AFU Data Record is exported
New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
ExportAfuFile¶
-
AfuManager.
ExportAfuFile
¶ Export all Data Records of an AFU to a RPCIII file
Signature
ExportAfuFile(afuFileName, exportFileName)
Parameters: - afuFileName (str) – AFU filename
- exportFileName (str) – Name of destination file to which AFU Data Record is exported
New in version NX5.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetAfuData¶
-
AfuManager.
GetAfuData
¶ Return data from an AFU Data Record
Signature
GetAfuData(afuFileName, recordIndex)
Parameters: - afuFileName (str) – AFU filename
- recordIndex (int) – Index of the AFU Data Record in the AFU file. Must begin with 1
Returns: a tuple
Return type: A tuple consisting of (recordTimestamp, afuData). recordTimestamp is a str. Time stamp string indicates the last time the AFU Data Record was edited afuData is a
NXOpen.CAE.AfuData
. AFU record data queriedNew in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetAfuUnitText¶
-
AfuManager.
GetAfuUnitText
¶ Return the unit text of AFU data like “mm”, “sec” etc.
Signature
GetAfuUnitText(unit)
Parameters: unit ( NXOpen.CAE.XyFunctionUnit
) – Unit Code of AFU dataReturns: Unit text of AFU data Return type: str New in version NX5.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetAfuUnitTypeText¶
-
AfuManager.
GetAfuUnitTypeText
¶ Return the unit type text of AFU data like “Displacement”, “Time” etc.
Signature
GetAfuUnitTypeText(unit)
Parameters: unit ( NXOpen.CAE.XyFunctionUnit
) – Unit Code of AFU dataReturns: Unit type text of AFU data Return type: str New in version NX5.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetRecordIndexes¶
-
AfuManager.
GetRecordIndexes
¶ Return indices of all Data Records in an AFU file
Signature
GetRecordIndexes(afuFileName)
Parameters: afuFileName (str) – AFU Filename Returns: Index array of all Data Records in the AFU file. Return type: list of int New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
ImportAfu¶
-
AfuManager.
ImportAfu
¶ Import AFU Data Records from a CSV, MAT, DAC or RPCIII file
Signature
ImportAfu(importFileName, afuFileName)
Parameters: - importFileName (str) – Filename for the file to be imported
- afuFileName (str) – AFU Filename to import data into
New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
ListFileInformation¶
-
AfuManager.
ListFileInformation
¶ List header information of all AFU Data Records in an AFU file to listing window or a specified output file
Signature
ListFileInformation(afuFileName, listPointData, outputFileName, mode)
Parameters: - afuFileName (str) – AFU filename
- listPointData (bool) – List Control Flag. If true, the record XY data will be listed. Otherwise only AFU header information is listed.
- outputFileName (str) – Output file to which the record information is written. If NULL, the information is only output to the listing window
- mode (
NXOpen.CAE.AfuManagerWritingFileMode
) – Overwrite or Append Output Mode for file output. Only valid when output file name is not NULL.
New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
ListRecordInformation¶
-
AfuManager.
ListRecordInformation
¶ List the AFU Data Record information to listing window or a specified output file
Signature
ListRecordInformation(afuFileName, recordIndex, listPointData, outputFileName, mode)
Parameters: - afuFileName (str) – AFU Filename
- recordIndex (int) – Index of the AFU Data Record to be listed
- listPointData (bool) – List control flag. If true, the record XY data will be listed. Otherwise only AFU header information is listed.
- outputFileName (str) – Output file to which the record information is written. If NULL, the information is only output to the listing window.
- mode (
NXOpen.CAE.AfuManagerWritingFileMode
) – Overwrite or Append Output Mode for file output. Only valid when output file name is not NULL.
New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
RenameRecord¶
-
AfuManager.
RenameRecord
¶ Rename an AFU Data Record
Signature
RenameRecord(afuFileName, recordIndex, newRecordName)
Parameters: - afuFileName (str) – AFU Filename
- recordIndex (int) – Index of the AFU Data Record in the AFU file. Must begin with 1.
- newRecordName (str) – New Data Record name
New in version NX4.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)