AfuDataAbscissaType Enumeration¶
NXOpen.CAE.AfuData.AbscissaType is an alias for NXOpen.CAE.AfuDataAbscissaType
-
class
NXOpen.CAE.
AfuDataAbscissaType
¶ Bases:
object
Defines abscissa data type for AFU data record
Enum Members
Enum Member Enum Member Description Even The abscissa value is even and calculated by incrementUneven The abscissa value is uneven and input by userSequence The abscissa value is a sequence and input by user. Please don’t use this value after NX9.0-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-