AfuManagerWritingFileMode Enumeration¶
NXOpen.CAE.AfuManager.WritingFileMode is an alias for NXOpen.CAE.AfuManagerWritingFileMode
-
class
NXOpen.CAE.
AfuManagerWritingFileMode
¶ Bases:
object
This enumeration defines the modes of outputting information to a file
Enum Members
Enum Member Enum Member Description Override Opens an empty file for writing. If the given file exists, its contents are destroyed.Append Opens a file for appending data to the end of the file-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-