AfuZHeaderInfo Class

class NXOpen.CAE.AfuZHeaderInfo

Bases: NXOpen.TransientObject

Represents the Z axis header information for an afu record

New in version NX10.0.0.

Properties

Property Description
GeneralValue Returns or sets the value of general field
OrderValue Returns or sets the value of order field
RpmValue Returns or sets the value of RPM field
TimeValue Returns or sets the value of time field
Unit Returns or sets the unit type of Z axis

Methods

Method Description
Dispose The object destructor

Property Detail

GeneralValue

AfuZHeaderInfo.GeneralValue

Returns or sets the value of general field

-------------------------------------

Getter Method

Signature GeneralValue()

Returns:the value of general field
Return type:float

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

-------------------------------------

Setter Method

Signature GeneralValue(generalValue)

Parameters:generalValue (float) – the value of general field

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

OrderValue

AfuZHeaderInfo.OrderValue

Returns or sets the value of order field

-------------------------------------

Getter Method

Signature OrderValue()

Returns:the value of order field
Return type:float

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

-------------------------------------

Setter Method

Signature OrderValue(orderValue)

Parameters:orderValue (float) – the value of order field

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

RpmValue

AfuZHeaderInfo.RpmValue

Returns or sets the value of RPM field

-------------------------------------

Getter Method

Signature RpmValue()

Returns:the value of RPM field
Return type:float

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

-------------------------------------

Setter Method

Signature RpmValue(rpmValue)

Parameters:rpmValue (float) – the value of RPM field

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

TimeValue

AfuZHeaderInfo.TimeValue

Returns or sets the value of time field

-------------------------------------

Getter Method

Signature TimeValue()

Returns:the value of time field
Return type:float

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

-------------------------------------

Setter Method

Signature TimeValue(timeValue)

Parameters:timeValue (float) – the value of time field

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

Unit

AfuZHeaderInfo.Unit

Returns or sets the unit type of Z axis

-------------------------------------

Getter Method

Signature Unit()

Returns:the unit type of Z axis
Return type:NXOpen.CAE.XyFunctionUnit

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

-------------------------------------

Setter Method

Signature Unit(unit)

Parameters:unit (NXOpen.CAE.XyFunctionUnit) – the unit type of Z axis

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

Method Detail

Dispose

AfuZHeaderInfo.Dispose

The object destructor

Signature Dispose()

New in version NX10.0.0.

License requirements: None.