ManualMorphBuilderMapType Enumeration

NXOpen.CAE.ManualMorphBuilder.MapType is an alias for NXOpen.CAE.ManualMorphBuilderMapType

class NXOpen.CAE.ManualMorphBuilderMapType

Bases: object

Represents the type of Manual Mapping

Enum Members

Enum Member Enum Member Description
Stationary
stationary mapping
NodeToPoint
node to point mapping
NodeToEdge
node to edge mapping
NodeToFace
node to face mapping
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.