PostScenarioVariantType Enumeration¶
-
class
NXOpen.CAE.
PostScenarioVariantType
¶ Bases:
object
The data type of a CAE.
PostScenarioVariant Value Enum Members
Enum Member Enum Member Description Boolean a boolean valueInteger an integer numberDouble a real numberComplex a complex numberString an ASCII character stringUnicodeString a Unicode UTF-8 character string-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-