AutomaticMorphBuilderOrphanNodeMovementType Enumeration

NXOpen.CAE.AutomaticMorphBuilder.OrphanNodeMovementType is an alias for NXOpen.CAE.AutomaticMorphBuilderOrphanNodeMovementType

class NXOpen.CAE.AutomaticMorphBuilderOrphanNodeMovementType

Bases: object

Orphan Node Movement Method - specify how the nodes move in topologically modified region.

Enum Members

Enum Member Enum Member Description
BasedOnNbrMovement
Based on adjacent nodes movement.
Stationary
Stationary in topologically modified region.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.