IBeamSectionBuilder Class

class NXOpen.CAE.IBeamSectionBuilder

Bases: NXOpen.Builder

Represents a NXOpen.CAE.IBeamSectionBuilder

This is an abstract class

New in version NX7.5.0.

Properties

Property Description
PropertyTable Returns the section builder’s NXOpen.CAE.PropertyTable
SectionName Returns or sets the section name
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
GetUserDefinedStressRecoveryPoints Gets the user-defined stress recovery points.
SetUserDefinedStressRecoveryPoints Sets the user-defined stress recovery points.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

PropertyTable

IBeamSectionBuilder.PropertyTable

Returns the section builder’s NXOpen.CAE.PropertyTable

-------------------------------------

Getter Method

Signature PropertyTable()

Returns:
Return type:NXOpen.CAE.PropertyTable

New in version NX7.5.0.

License requirements: None.

SectionName

IBeamSectionBuilder.SectionName

Returns or sets the section name

-------------------------------------

Getter Method

Signature SectionName()

Returns:
Return type:str

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SectionName(sectionName)

Parameters:sectionName (str) –

New in version NX7.5.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

Method Detail

GetUserDefinedStressRecoveryPoints

IBeamSectionBuilder.GetUserDefinedStressRecoveryPoints

Gets the user-defined stress recovery points.

Signature GetUserDefinedStressRecoveryPoints()

Returns:
Return type:list of NXOpen.Point2d

New in version NX7.5.0.

License requirements: None.

SetUserDefinedStressRecoveryPoints

IBeamSectionBuilder.SetUserDefinedStressRecoveryPoints

Sets the user-defined stress recovery points.

Signature SetUserDefinedStressRecoveryPoints(points)

Parameters:points (list of NXOpen.Point2d) –

New in version NX7.5.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

Validate

IBeamSectionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.