LaminatePlyGroupLink Enumeration¶
NXOpen.CAE.LaminatePlyGroup.Link is an alias for NXOpen.CAE.LaminatePlyGroupLink
-
class
NXOpen.CAE.
LaminatePlyGroupLink
¶ Bases:
object
Used to specify the kind of linked group created
Enum Members
Enum Member Enum Member Description NotSet not a linked groupRepeat same ply layupSymm symmetric layupAnti symmetric layup with reversed anglesRev same layup with reversed angles-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-