CfdLocalResolutionConstraintCollection Class¶
-
class
NXOpen.CAE.
CfdLocalResolutionConstraintCollection
¶ Bases:
object
Provides methods for managing Local Resolution Constraints:py:class:CAE.CfdLocalResolutionConstraint in a fem part
To obtain an instance of this class, refer to
NXOpen.CAE.BaseFEModel
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CloneConstraint | Clones a local resolution constraint. |
CreateBuilder | Creates a local resolution constraint builder @return LocalResolutionConstraint Builder |
DeleteConstraint | Delete a local resolution constraint. |
Find | Finds the CAE.CfdLocalResolutionConstraint with the given identifier as recorded in a journal. |
FindObject | Finds the CAE.CfdLocalResolutionConstraint with the given identifier as recorded in a journal. |
Method Detail¶
CloneConstraint¶
-
CfdLocalResolutionConstraintCollection.
CloneConstraint
¶ Clones a local resolution constraint.
Signature
CloneConstraint(source)
Parameters: source ( NXOpen.CAE.CfdLocalResolutionConstraint
) – Source local resolution constraintReturns: Cloned local resolution constraint Return type: NXOpen.CAE.CfdLocalResolutionConstraint
New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
CreateBuilder¶
-
CfdLocalResolutionConstraintCollection.
CreateBuilder
¶ Creates a local resolution constraint builder
Signature
CreateBuilder(recipe)
Parameters: recipe ( NXOpen.TaggedObject
) –CfdLocalResolutionConstraint
to be edited, if None orFluidDomainRecipe
then create a new oneReturns: LocalResolutionConstraint Builder Return type: NXOpen.CAE.CfdLocalResolutionConstraintBuilder
New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
DeleteConstraint¶
-
CfdLocalResolutionConstraintCollection.
DeleteConstraint
¶ Delete a local resolution constraint.
Signature
DeleteConstraint(constraint)
Parameters: constraint ( NXOpen.CAE.CfdLocalResolutionConstraint
) – The local resolution constraint to be deletedNew in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
Find¶
-
CfdLocalResolutionConstraintCollection.
Find
¶ Finds the
CAE.CfdLocalResolutionConstraint
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when Find is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with the given journal identifier.
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Local Resolution Constraint name Returns: local resolution constraint with this identifier Return type: NXOpen.CAE.CfdLocalResolutionConstraint
New in version NX11.0.0.
License requirements: None.
FindObject¶
-
CfdLocalResolutionConstraintCollection.
FindObject
¶ Finds the
CAE.CfdLocalResolutionConstraint
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Local Resolution Constraint name Returns: local resolution constraint with this identifier Return type: NXOpen.CAE.CfdLocalResolutionConstraint
New in version NX9.0.0.
License requirements: None.