CfdLocalResolutionConstraintBuilder Class¶
-
class
NXOpen.CAE.
CfdLocalResolutionConstraintBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.CfdLocalResolutionConstraint
builderTo create a new instance of this class, use
NXOpen.CAE.CfdLocalResolutionConstraintCollection.CreateBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
BboxPoint | Returns or sets the bbox point |
BsphereRadius | Returns the bsphere radius |
LocalResolution | Returns the local resolution |
LocalSubdivision | Returns or sets the local subdivision |
NameString | Returns or sets the name string |
PointSelection | Returns or sets the point selection |
PriorityLevel | Returns or sets the priority level |
ResolutionDensityType | Returns or sets the resolution density type |
SelectElement | Returns the selected shell element |
SelectObject | Returns the select object |
SizingOption | Returns or sets the sizing option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CfdLocalResolutionConstraintBuilderLocalSubdivisions Enumeration | The local subdivision. |
CfdLocalResolutionConstraintBuilderPriority Enumeration | The priority level. |
CfdLocalResolutionConstraintBuilderResolutionDensity Enumeration | The Resolution density type. |
CfdLocalResolutionConstraintBuilderSizing Enumeration | The sizing option. |
Property Detail¶
BboxPoint¶
-
CfdLocalResolutionConstraintBuilder.
BboxPoint
¶ Returns or sets the bbox point
-------------------------------------
Getter Method
Signature
BboxPoint()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BboxPoint(bboxPoint)
Parameters: bboxPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
BsphereRadius¶
-
CfdLocalResolutionConstraintBuilder.
BsphereRadius
¶ Returns the bsphere radius
-------------------------------------
Getter Method
Signature
BsphereRadius()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
LocalResolution¶
-
CfdLocalResolutionConstraintBuilder.
LocalResolution
¶ Returns the local resolution
-------------------------------------
Getter Method
Signature
LocalResolution()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
LocalSubdivision¶
-
CfdLocalResolutionConstraintBuilder.
LocalSubdivision
¶ Returns or sets the local subdivision
-------------------------------------
Getter Method
Signature
LocalSubdivision()
Returns: Return type: NXOpen.CAE.CfdLocalResolutionConstraintBuilderLocalSubdivisions
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocalSubdivision(localSubdivision)
Parameters: localSubdivision ( NXOpen.CAE.CfdLocalResolutionConstraintBuilderLocalSubdivisions
) –New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
NameString¶
-
CfdLocalResolutionConstraintBuilder.
NameString
¶ Returns or sets the name string
-------------------------------------
Getter Method
Signature
NameString()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NameString(nameString)
Parameters: nameString (str) – New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
PointSelection¶
-
CfdLocalResolutionConstraintBuilder.
PointSelection
¶ Returns or sets the point selection
-------------------------------------
Getter Method
Signature
PointSelection()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSelection(pointSelection)
Parameters: pointSelection ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
PriorityLevel¶
-
CfdLocalResolutionConstraintBuilder.
PriorityLevel
¶ Returns or sets the priority level
-------------------------------------
Getter Method
Signature
PriorityLevel()
Returns: Return type: NXOpen.CAE.CfdLocalResolutionConstraintBuilderPriority
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriorityLevel(priorityLevel)
Parameters: priorityLevel ( NXOpen.CAE.CfdLocalResolutionConstraintBuilderPriority
) –New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
ResolutionDensityType¶
-
CfdLocalResolutionConstraintBuilder.
ResolutionDensityType
¶ Returns or sets the resolution density type
-------------------------------------
Getter Method
Signature
ResolutionDensityType()
Returns: Return type: NXOpen.CAE.CfdLocalResolutionConstraintBuilderResolutionDensity
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResolutionDensityType(resolutionDensityType)
Parameters: resolutionDensityType ( NXOpen.CAE.CfdLocalResolutionConstraintBuilderResolutionDensity
) –New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
SelectElement¶
-
CfdLocalResolutionConstraintBuilder.
SelectElement
¶ Returns the selected shell element
-------------------------------------
Getter Method
Signature
SelectElement()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX11.0.0.
License requirements: None.
SelectObject¶
-
CfdLocalResolutionConstraintBuilder.
SelectObject
¶ Returns the select object
-------------------------------------
Getter Method
Signature
SelectObject()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX9.0.0.
License requirements: None.
SizingOption¶
-
CfdLocalResolutionConstraintBuilder.
SizingOption
¶ Returns or sets the sizing option
-------------------------------------
Getter Method
Signature
SizingOption()
Returns: Return type: NXOpen.CAE.CfdLocalResolutionConstraintBuilderSizing
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizingOption(sizingOption)
Parameters: sizingOption ( NXOpen.CAE.CfdLocalResolutionConstraintBuilderSizing
) –New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
Method Detail¶
Validate¶
-
CfdLocalResolutionConstraintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.