GraphFromResultProbeBuilder Class¶
-
class
NXOpen.CAE.
GraphFromResultProbeBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.GraphFromResultProbeBuilder
This is an abstract class and cannot be instantiated
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetPlotType | The plot type will be set |
SetResultProbes | The plot type will be set |
SetViewIndex | The view index will be set |
SetWindowIndex | The window index will be set |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GraphFromResultProbeBuilderPlotType Enumeration | Defines the Plot Type options |
Method Detail¶
SetPlotType¶
-
GraphFromResultProbeBuilder.
SetPlotType
¶ The plot type will be set
Signature
SetPlotType(plotType)
Parameters: plotType ( NXOpen.CAE.GraphFromResultProbeBuilderPlotType
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultProbes¶
-
GraphFromResultProbeBuilder.
SetResultProbes
¶ The plot type will be set
Signature
SetResultProbes(resultProbes)
Parameters: resultProbes (list of NXOpen.CAE.ResultProbe
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetViewIndex¶
-
GraphFromResultProbeBuilder.
SetViewIndex
¶ The view index will be set
Signature
SetViewIndex(viewIndex)
Parameters: viewIndex (int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetWindowIndex¶
-
GraphFromResultProbeBuilder.
SetWindowIndex
¶ The window index will be set
Signature
SetWindowIndex(windowIndex)
Parameters: windowIndex (int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
GraphFromResultProbeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.