DurabilityStressAxesBuilderStressAxisMethodEnum Enumeration

NXOpen.CAE.DurabilityStressAxesBuilder.StressAxisMethodEnum is an alias for NXOpen.CAE.DurabilityStressAxesBuilderStressAxisMethodEnum

class NXOpen.CAE.DurabilityStressAxesBuilderStressAxisMethodEnum

Bases: object

the Stress Axis Method Enum.

Enum Members

Enum Member Enum Member Description
ElementFace
Element Face
NodalUniAxial
Nodal Uni Axial
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.