ProjectNodesToCadGeometryBuilder Class¶
-
class
NXOpen.CAE.
ProjectNodesToCadGeometryBuilder
¶ Bases:
NXOpen.Builder
Allows you to query the mesh nodes that are off the underlying Cad geometry by a given tolerance, and if requested this builder can adjust the node locations to put them back on to the underlying Cad geometry.
To create a new instance of this class, use
NXOpen.CAE.MeshManager.CreateProjectNodesToCadGeometryBuilder()
New in version NX6.0.4.
Properties¶
Property | Description |
---|---|
AdjustedNodeLocationColor | Returns or sets the display color of proximity node new location which will meet the given tolerance with undelying CAD geometry. |
CheckedObjectsList | Returns the selected objects for checking. |
IncludeMidnodes | Returns or sets a value indicating whether to include element midnodes in the operation. |
ListingOptionState | Returns or sets the listing option |
OperationState | Returns or sets the operation to be performed. |
OriginalNodeLocationColor | Returns or sets the display color of proximity nodes’ original location. |
ProximityTolerance | Returns or sets the proximity tolerance used to determine if nodes on close enough to be considered on the CAD geometry |
SelectionList | Returns the selected meshes |
ShowNodeLabels | Returns or sets a value indicating whether to show the labels for proximity nodes are off underlying CAD geometry. |
ShowNodeLocations | Returns or sets a value indicating whether to show original location and adjusted location for the proximity nodes that are off the underlying CAD geometry by a given tolerance. |
Tag | Returns the Tag for this object. |
Tolerance | Returns the proximity tolerance used to determine if nodes on close enough to be considered on the CAD geometry |
Methods¶
Method | Description |
---|---|
AdjustProximityNodes | Adjusts the proximity nodes identified to the new location to meet the given tolerance with underlying CAD geometries. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetNodes | Returns the cached nodes calculated by CAE.ProjectNodesToCadGeometryBuilder.IdentifyCadGeometry() . |
GetObject | Returns the object currently being edited by this builder. |
GetProximityNodes | Returns the cached proximity nodes calculated by CAE.ProjectNodesToCadGeometryBuilder.IdentifyProximityNodes() . |
IdentifyCadGeometry | Identifies the relationship between CAD geometry and the nodes, The identified result will be cached, you could access the cached results by calling CAE.ProjectNodesToCadGeometryBuilder.GetNodes() . |
IdentifyProximityNodes | Identifies the proximity nodes which are off the underlying CAD geometry according to CAE.ProjectNodesToCadGeometryBuilder.ProximityTolerance`() and CAE.ProjectNodesToCadGeometryBuilder.IncludeMidnodes`() . |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ProjectNodesToCadGeometryBuilderListingOption Enumeration | Listing Options |
ProjectNodesToCadGeometryBuilderOperation Enumeration | Operations |
Property Detail¶
AdjustedNodeLocationColor¶
-
ProjectNodesToCadGeometryBuilder.
AdjustedNodeLocationColor
¶ Returns or sets the display color of proximity node new location which will meet the given tolerance with undelying CAD geometry.
-------------------------------------
Getter Method
Signature
AdjustedNodeLocationColor()
Returns: Return type: Id New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjustedNodeLocationColor(locationColor)
Parameters: locationColor (Id) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CheckedObjectsList¶
-
ProjectNodesToCadGeometryBuilder.
CheckedObjectsList
¶ Returns the selected objects for checking.
The objects must be
CAE.Mesh
,CAE.CAEBody
orCAE.CAEFace
-------------------------------------
Getter Method
Signature
CheckedObjectsList()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
IncludeMidnodes¶
-
ProjectNodesToCadGeometryBuilder.
IncludeMidnodes
¶ Returns or sets a value indicating whether to include element midnodes in the operation.
-------------------------------------
Getter Method
Signature
IncludeMidnodes()
Returns: Return type: bool New in version NX6.0.4.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
IncludeMidnodes(bIncludeMidnodes)
Parameters: bIncludeMidnodes (bool) – New in version NX6.0.4.
License requirements: nx_masterfem (“Finite Element Modeling”)
ListingOptionState¶
-
ProjectNodesToCadGeometryBuilder.
ListingOptionState
¶ Returns or sets the listing option
-------------------------------------
Getter Method
Signature
ListingOptionState()
Returns: Return type: NXOpen.CAE.ProjectNodesToCadGeometryBuilderListingOption
New in version NX6.0.4.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
ListingOptionState(option)
Parameters: option ( NXOpen.CAE.ProjectNodesToCadGeometryBuilderListingOption
) –New in version NX6.0.4.
License requirements: nx_masterfem (“Finite Element Modeling”)
OperationState¶
-
ProjectNodesToCadGeometryBuilder.
OperationState
¶ Returns or sets the operation to be performed.
-------------------------------------
Getter Method
Signature
OperationState()
Returns: Return type: NXOpen.CAE.ProjectNodesToCadGeometryBuilderOperation
New in version NX6.0.4.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
OperationState(operation)
Parameters: operation ( NXOpen.CAE.ProjectNodesToCadGeometryBuilderOperation
) –New in version NX6.0.4.
License requirements: nx_masterfem (“Finite Element Modeling”)
OriginalNodeLocationColor¶
-
ProjectNodesToCadGeometryBuilder.
OriginalNodeLocationColor
¶ Returns or sets the display color of proximity nodes’ original location.
-------------------------------------
Getter Method
Signature
OriginalNodeLocationColor()
Returns: Return type: Id New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OriginalNodeLocationColor(locationColor)
Parameters: locationColor (Id) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ProximityTolerance¶
-
ProjectNodesToCadGeometryBuilder.
ProximityTolerance
¶ Returns or sets the proximity tolerance used to determine if nodes on close enough to be considered on the CAD geometry
-------------------------------------
Getter Method
Signature
ProximityTolerance()
Returns: Return type: float New in version NX6.0.4.
Deprecated since version NX8.5.0: Use
CAE.ProjectNodesToCadGeometryBuilder.Tolerance()
instead.License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
ProximityTolerance(dProximityTolerance)
Parameters: dProximityTolerance (float) – New in version NX6.0.4.
Deprecated since version NX8.5.0: Use
CAE.ProjectNodesToCadGeometryBuilder.Tolerance()
instead.License requirements: nx_masterfem (“Finite Element Modeling”)
SelectionList¶
-
ProjectNodesToCadGeometryBuilder.
SelectionList
¶ Returns the selected meshes
-------------------------------------
Getter Method
Signature
SelectionList()
Returns: Return type: NXOpen.CAE.SelectMeshList
New in version NX6.0.4.
Deprecated since version NX8.5.0: Use
CAE.ProjectNodesToCadGeometryBuilder.CheckedObjectsList()
instead.License requirements: nx_masterfem (“Finite Element Modeling”)
ShowNodeLabels¶
-
ProjectNodesToCadGeometryBuilder.
ShowNodeLabels
¶ Returns or sets a value indicating whether to show the labels for proximity nodes are off underlying CAD geometry.
-------------------------------------
Getter Method
Signature
ShowNodeLabels()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowNodeLabels(showLabels)
Parameters: showLabels (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ShowNodeLocations¶
-
ProjectNodesToCadGeometryBuilder.
ShowNodeLocations
¶ Returns or sets a value indicating whether to show original location and adjusted location for the proximity nodes that are off the underlying CAD geometry by a given tolerance.
The original node location will be displayed in color
CAE.ProjectNodesToCadGeometryBuilder.OriginalNodeLocationColor`()
. The adjusted node location will be displayed in colorCAE.ProjectNodesToCadGeometryBuilder.AdjustedNodeLocationColor`()
.-------------------------------------
Getter Method
Signature
ShowNodeLocations()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowNodeLocations(showLocations)
Parameters: showLocations (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Tolerance¶
-
ProjectNodesToCadGeometryBuilder.
Tolerance
¶ Returns the proximity tolerance used to determine if nodes on close enough to be considered on the CAD geometry
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Method Detail¶
AdjustProximityNodes¶
-
ProjectNodesToCadGeometryBuilder.
AdjustProximityNodes
¶ Adjusts the proximity nodes identified to the new location to meet the given tolerance with underlying CAD geometries.
The cached identified result will be clean when the adjust work is completed. The method
Builder.Commit()
will do the same thing. The adjust work is only available when the context part of this builder is aCAE.FemPart
.Signature
AdjustProximityNodes()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetNodes¶
-
ProjectNodesToCadGeometryBuilder.
GetNodes
¶ Returns the cached nodes calculated by
CAE.ProjectNodesToCadGeometryBuilder.IdentifyCadGeometry()
.Signature
GetNodes()
Returns: a tuple Return type: A tuple consisting of (projectLocations, nodes, cadGeometries). projectLocations is a list of NXOpen.Point3d
. nodes is a list ofNXOpen.CAE.FENode
. cadGeometries is a list ofNXOpen.NXObject
.New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetProximityNodes¶
-
ProjectNodesToCadGeometryBuilder.
GetProximityNodes
¶ Returns the cached proximity nodes calculated by
CAE.ProjectNodesToCadGeometryBuilder.IdentifyProximityNodes()
.Signature
GetProximityNodes()
Returns: a tuple Return type: A tuple consisting of (projectLocations, proximityNodes). projectLocations is a list of NXOpen.Point3d
. proximityNodes is a list ofNXOpen.CAE.FENode
.New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
IdentifyCadGeometry¶
-
ProjectNodesToCadGeometryBuilder.
IdentifyCadGeometry
¶ Identifies the relationship between CAD geometry and the nodes, The identified result will be cached, you could access the cached results by calling
CAE.ProjectNodesToCadGeometryBuilder.GetNodes()
.Old cached results are automatically cleaned up when the new identify process is running.
Signature
IdentifyCadGeometry()
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
IdentifyProximityNodes¶
-
ProjectNodesToCadGeometryBuilder.
IdentifyProximityNodes
¶ Identifies the proximity nodes which are off the underlying CAD geometry according to
CAE.ProjectNodesToCadGeometryBuilder.ProximityTolerance`()
andCAE.ProjectNodesToCadGeometryBuilder.IncludeMidnodes`()
.If showing nodes is true, the identified node location will be displayed. The identified result will be cached, you could access the cached identified nodes by
CAE.ProjectNodesToCadGeometryBuilder.GetProximityNodes()
. Each time, the old cached result will be clean up when the new identify process is running.Signature
IdentifyProximityNodes()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
ProjectNodesToCadGeometryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.