FENode Class

class NXOpen.CAE.FENode

Bases: NXOpen.TaggedObject, NXOpen.IFitTo, NXOpen.CAE.IExportableFEEntity

Represents a Finite Element Node.

New in version NX7.5.0.

Properties

Property Description
Coordinates Returns the node cooridnates in absolute space
DisplacementCsys Returns the nodes displacement coordinate system or None if it is the absolute coordinate system
IsOccurrence Returns whether this object is an occurrence or not.
JournalIdentifier Returns the identifier that would be recorded in a journal for this object.
Label Returns the node label
Name Returns the custom name of the object.
OwningComponent Returns the owning component, if this object is an occurrence.
OwningPart Returns the owning part of this object
Prototype Returns the prototype of this object if it is an occurrence.
ReferenceCsys Returns the nodes reference coordinate system or None if it is the absolute coordinate system
Tag Returns the Tag for this object.

Methods

Method Description
FindObject Finds the NXOpen.NXObject with the given identifier as recorded in a journal.
GetElements Returns the elements which refer to this node @return
GetSolverCardSyntax Returns the solver card syntax strings for this entity.
Print Prints a representation of this object to the system log file.
SetName Sets the custom name of the object.

Property Detail

Coordinates

FENode.Coordinates

Returns the node cooridnates in absolute space

-------------------------------------

Getter Method

Signature Coordinates()

Returns:
Return type:NXOpen.Point3d

New in version NX7.5.2.

License requirements: None.

DisplacementCsys

FENode.DisplacementCsys

Returns the nodes displacement coordinate system or None if it is the absolute coordinate system

-------------------------------------

Getter Method

Signature DisplacementCsys()

Returns:
Return type:NXOpen.CoordinateSystem

New in version NX7.5.2.

License requirements: None.

IsOccurrence

FENode.IsOccurrence

Returns whether this object is an occurrence or not.

-------------------------------------

Getter Method

Signature IsOccurrence()

Returns:This object is an occurrence
Return type:bool

New in version NX3.0.0.

License requirements: None.

JournalIdentifier

FENode.JournalIdentifier

Returns the identifier that would be recorded in a journal for this object.

This may not be the same across different releases of the software.

-------------------------------------

Getter Method

Signature JournalIdentifier()

Returns:
Return type:str

New in version NX3.0.0.

License requirements: None.

Label

FENode.Label

Returns the node label

-------------------------------------

Getter Method

Signature Label()

Returns:
Return type:int

New in version NX7.5.2.

License requirements: None.

Name

FENode.Name

Returns the custom name of the object.

-------------------------------------

Getter Method

Signature Name()

Returns:
Return type:str

New in version NX3.0.0.

License requirements: None.

OwningComponent

FENode.OwningComponent

Returns the owning component, if this object is an occurrence.

-------------------------------------

Getter Method

Signature OwningComponent()

Returns:
Return type:NXOpen.Assemblies.Component

New in version NX3.0.0.

License requirements: None.

OwningPart

FENode.OwningPart

Returns the owning part of this object

-------------------------------------

Getter Method

Signature OwningPart()

Returns:The owning part of this object or null if it does not have an owner
Return type:NXOpen.BasePart

New in version NX3.0.0.

License requirements: None.

Prototype

FENode.Prototype

Returns the prototype of this object if it is an occurrence.

-------------------------------------

Getter Method

Signature Prototype()

Returns:The prototype of this object or null if this object is not an occurrence
Return type:NXOpen.INXObject

New in version NX3.0.0.

License requirements: None.

ReferenceCsys

FENode.ReferenceCsys

Returns the nodes reference coordinate system or None if it is the absolute coordinate system

-------------------------------------

Getter Method

Signature ReferenceCsys()

Returns:
Return type:NXOpen.CoordinateSystem

New in version NX7.5.2.

License requirements: None.

Method Detail

FindObject

FENode.FindObject

Finds the NXOpen.NXObject with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Journal identifier of the object
Returns:
Return type:NXOpen.INXObject

New in version NX3.0.0.

License requirements: None.

GetElements

FENode.GetElements

Returns the elements which refer to this node

Signature GetElements()

Returns:
Return type:list of NXOpen.CAE.FEElement

New in version NX7.5.2.

License requirements: None.

GetSolverCardSyntax

FENode.GetSolverCardSyntax

Returns the solver card syntax strings for this entity.

Signature GetSolverCardSyntax()

Returns:
Return type:list of str

New in version NX8.5.0.

License requirements: None.

Print

FENode.Print

Prints a representation of this object to the system log file.

Signature Print()

New in version NX3.0.0.

License requirements: None.

SetName

FENode.SetName

Sets the custom name of the object.

NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.

Signature SetName(name)

Parameters:name (str) –

New in version NX3.0.0.

License requirements: None.