FEElement Class¶
-
class
NXOpen.CAE.
FEElement
¶ Bases:
NXOpen.TaggedObject
,NXOpen.IFitTo
,NXOpen.CAE.IExportableFEEntity
Represents a Finite Element.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Label | Returns the element label |
Mesh | Returns the mesh for this element |
Name | Returns the custom name of the object. |
NumberOfCornerNodes | Returns the number of corner nodes |
Order | Returns the element order |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Shape | Returns the element shape |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetCornerNodesOnEdge | Returns the corner nodes for this element edge. |
GetCornerNodesOnFace | Returns the corner nodes for this element face @return |
GetElemEdge | Returns an element edge NXOpen.CAE.FEElemEdge given the element and edge id @return |
GetElemFace | Returns an element face NXOpen.CAE.FEElemFace given the element and face id @return |
GetFaceNormal | Returns the normal vector for an element face @return |
GetMidNodeOnEdge | Returns the mid node for this element edge, if the element order CAE.FEElement.Order() is CAE.ElementTypesOrder.Mixed or an order that does not support mid nodes, then the node returned may be None. |
GetMidNodesOnFace | Returns the mid nodes for this element face, if the element order CAE.FEElement.Order() is CAE.ElementTypesOrder.Mixed , then some of the nodes returned may be None. |
GetNodes | Returns the nodes for this element, if the element order CAE.FEElement.Order() is mixed order, some of the mid nodes returned may be None. |
GetNumberOfCornerNodesOnEdge | Returns the number of corner nodes on element edge @return |
GetNumberOfCornerNodesOnFace | Returns the number of corner nodes on element face @return |
GetSolverCardSyntax | Returns the solver card syntax strings for this entity. |
Prints a representation of this object to the system log file. | |
SetName | Sets the custom name of the object. |
Property Detail¶
IsOccurrence¶
-
FEElement.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
FEElement.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Label¶
-
FEElement.
Label
¶ Returns the element label
-------------------------------------
Getter Method
Signature
Label()
Returns: Return type: int New in version NX7.5.2.
License requirements: None.
Mesh¶
-
FEElement.
Mesh
¶ Returns the mesh for this element
-------------------------------------
Getter Method
Signature
Mesh()
Returns: Return type: NXOpen.CAE.Mesh
New in version NX7.5.2.
License requirements: None.
Name¶
-
FEElement.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
NumberOfCornerNodes¶
-
FEElement.
NumberOfCornerNodes
¶ Returns the number of corner nodes
-------------------------------------
Getter Method
Signature
NumberOfCornerNodes()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
Order¶
-
FEElement.
Order
¶ Returns the element order
-------------------------------------
Getter Method
Signature
Order()
Returns: Return type: NXOpen.CAE.ElementTypesOrder
New in version NX7.5.2.
License requirements: None.
OwningComponent¶
-
FEElement.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FEElement.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
FEElement.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Shape¶
-
FEElement.
Shape
¶ Returns the element shape
-------------------------------------
Getter Method
Signature
Shape()
Returns: Return type: NXOpen.CAE.ElementTypesShape
New in version NX7.5.2.
License requirements: None.
Method Detail¶
FindObject¶
-
FEElement.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetCornerNodesOnEdge¶
-
FEElement.
GetCornerNodesOnEdge
¶ Returns the corner nodes for this element edge.
Signature
GetCornerNodesOnEdge(edgeIndex)
Parameters: edgeIndex (int) – Returns: Return type: list of NXOpen.CAE.FENode
New in version NX11.0.0.
License requirements: None.
GetCornerNodesOnFace¶
-
FEElement.
GetCornerNodesOnFace
¶ Returns the corner nodes for this element face
Signature
GetCornerNodesOnFace(faceIndex)
Parameters: faceIndex (int) – Returns: Return type: list of NXOpen.CAE.FENode
New in version NX11.0.0.
License requirements: None.
GetElemEdge¶
-
FEElement.
GetElemEdge
¶ Returns an element edge
NXOpen.CAE.FEElemEdge
given the element and edge idSignature
GetElemEdge(edgeIndex)
Parameters: edgeIndex (int) – Returns: Return type: NXOpen.CAE.FEElemEdge
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetElemFace¶
-
FEElement.
GetElemFace
¶ Returns an element face
NXOpen.CAE.FEElemFace
given the element and face idSignature
GetElemFace(faceIndex)
Parameters: faceIndex (int) – Returns: Return type: NXOpen.CAE.FEElemFace
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetFaceNormal¶
-
FEElement.
GetFaceNormal
¶ Returns the normal vector for an element face
Signature
GetFaceNormal(faceIndex)
Parameters: faceIndex (int) – Returns: Return type: NXOpen.Vector3d
New in version NX11.0.0.
License requirements: None.
GetMidNodeOnEdge¶
-
FEElement.
GetMidNodeOnEdge
¶ Returns the mid node for this element edge, if the element order
CAE.FEElement.Order()
isCAE.ElementTypesOrder.Mixed
or an order that does not support mid nodes, then the node returned may be None.Signature
GetMidNodeOnEdge(edgeIndex)
Parameters: edgeIndex (int) – Returns: Return type: NXOpen.CAE.FENode
New in version NX11.0.0.
License requirements: None.
GetMidNodesOnFace¶
-
FEElement.
GetMidNodesOnFace
¶ Returns the mid nodes for this element face, if the element order
CAE.FEElement.Order()
isCAE.ElementTypesOrder.Mixed
, then some of the nodes returned may be None.If the Element Order does not support mid nodes nothing will be returned.
Signature
GetMidNodesOnFace(faceIndex)
Parameters: faceIndex (int) – Returns: Return type: list of NXOpen.CAE.FENode
New in version NX11.0.0.
License requirements: None.
GetNodes¶
-
FEElement.
GetNodes
¶ Returns the nodes for this element, if the element order
CAE.FEElement.Order()
is mixed order, some of the mid nodes returned may be None.When mid nodes are returned they will come after the corner nodes
Signature
GetNodes()
Returns: Return type: list of NXOpen.CAE.FENode
New in version NX7.5.2.
License requirements: None.
GetNumberOfCornerNodesOnEdge¶
-
FEElement.
GetNumberOfCornerNodesOnEdge
¶ Returns the number of corner nodes on element edge
Signature
GetNumberOfCornerNodesOnEdge(edgeIndex)
Parameters: edgeIndex (int) – Returns: Return type: int New in version NX11.0.0.
License requirements: None.
GetNumberOfCornerNodesOnFace¶
-
FEElement.
GetNumberOfCornerNodesOnFace
¶ Returns the number of corner nodes on element face
Signature
GetNumberOfCornerNodesOnFace(faceIndex)
Parameters: faceIndex (int) – Returns: Return type: int New in version NX11.0.0.
License requirements: None.
GetSolverCardSyntax¶
-
FEElement.
GetSolverCardSyntax
¶ Returns the solver card syntax strings for this entity.
Signature
GetSolverCardSyntax()
Returns: Return type: list of str New in version NX8.5.0.
License requirements: None.
Print¶
-
FEElement.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
FEElement.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.