ElementTypesOrder Enumeration

NXOpen.CAE.ElementTypes.Order is an alias for NXOpen.CAE.ElementTypesOrder

class NXOpen.CAE.ElementTypesOrder

Bases: object

Specifies different CAE Element Order types

Enum Members

Enum Member Enum Member Description
Undefined
Undefined
Linear
Linear
Parabolic
Parabolic
Mixed
Mixed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.