BcLabelManagerBuilder Class¶
-
class
NXOpen.CAE.
BcLabelManagerBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.BcLabelManagerBuilder
builder which can be used to renumberNXOpen.CAE.SimBC
id.This is limited to
NXOpen.CAE.SimBC
objects in the active solution. To create a new instance of this class, useNXOpen.CAE.SimSimulation.CreateBcLabelManagerBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
NumOfBc | Returns or sets a value indicating the number of BC to renumber |
RenumberMethod | Returns or sets a value indicating renumber method |
RenumberStartValue | Returns or sets a value indicating the number to offset by or renumber from |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetBcTags | A value indicating the list of tags of BC to renumber |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetBcTags | Sets tags of BC to renumber |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BcLabelManagerBuilderRenumberType Enumeration | Renumber Method |
Property Detail¶
NumOfBc¶
-
BcLabelManagerBuilder.
NumOfBc
¶ Returns or sets a value indicating the number of BC to renumber
-------------------------------------
Getter Method
Signature
NumOfBc()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumOfBc(numOfBc)
Parameters: numOfBc (int) – New in version NX11.0.0.
License requirements: None.
RenumberMethod¶
-
BcLabelManagerBuilder.
RenumberMethod
¶ Returns or sets a value indicating renumber method
-------------------------------------
Getter Method
Signature
RenumberMethod()
Returns: Return type: NXOpen.CAE.BcLabelManagerBuilderRenumberType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RenumberMethod(renumberMethod)
Parameters: renumberMethod ( NXOpen.CAE.BcLabelManagerBuilderRenumberType
) –New in version NX11.0.0.
License requirements: None.
RenumberStartValue¶
-
BcLabelManagerBuilder.
RenumberStartValue
¶ Returns or sets a value indicating the number to offset by or renumber from
-------------------------------------
Getter Method
Signature
RenumberStartValue()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RenumberStartValue(renumberStartValue)
Parameters: renumberStartValue (int) – New in version NX11.0.0.
License requirements: None.
Method Detail¶
GetBcTags¶
-
BcLabelManagerBuilder.
GetBcTags
¶ A value indicating the list of tags of BC to renumber
Signature
GetBcTags()
Returns: Return type: list of NXOpen.CAE.SimBC
New in version NX11.0.0.
License requirements: None.
SetBcTags¶
-
BcLabelManagerBuilder.
SetBcTags
¶ Sets tags of BC to renumber
Signature
SetBcTags(bcTags)
Parameters: bcTags (list of NXOpen.CAE.SimBC
) –New in version NX11.0.0.
License requirements: None.
Validate¶
-
BcLabelManagerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.