CAEConnectionBuilderMethodTypeEnum Enumeration¶
NXOpen.CAE.CAEConnectionBuilder.MethodTypeEnum is an alias for NXOpen.CAE.CAEConnectionBuilderMethodTypeEnum
-
class
NXOpen.CAE.
CAEConnectionBuilderMethodTypeEnum
¶ Bases:
object
the method of connection to be created
Enum Members
Enum Member Enum Member Description Proximity Based on proximityOrderOfSelection In order of selectionMeanVector Based on Mean VectorSortXcoord Based on sorted X coordinatesSortYcoord Based on sorted Y coordinatesSortZcoord Based on sorted Z coordinatesRbe3ToEdgeNodes Create spider element using projected node and edge nodesRbe3ToFaceNodes Create spider element using projected node and adjacent face nodes-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-