DurabilityLoadPatternBuilder Class

class NXOpen.CAE.DurabilityLoadPatternBuilder

Bases: NXOpen.CAE.DurabilityExcitationBuilder

Represents a CAE.DurabilityLoadPattern builder.

There is no kf creator for this.

New in version NX7.5.0.

Properties

Property Description
ExcitationName Returns or sets the excitation name.
Iteration Returns or sets the iteration.
Loadcase Returns or sets the load case.
Offset Returns or sets the offset.
PatternType Returns or sets the pattern type.
Scale Returns or sets the scale.
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Iteration

DurabilityLoadPatternBuilder.Iteration

Returns or sets the iteration.

-------------------------------------

Getter Method

Signature Iteration()

Returns:
Return type:int

New in version NX9.0.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature Iteration(iteration)

Parameters:iteration (int) –

New in version NX9.0.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Loadcase

DurabilityLoadPatternBuilder.Loadcase

Returns or sets the load case.

-------------------------------------

Getter Method

Signature Loadcase()

Returns:
Return type:int

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature Loadcase(loadcase)

Parameters:loadcase (int) –

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Offset

DurabilityLoadPatternBuilder.Offset

Returns or sets the offset.

-------------------------------------

Getter Method

Signature Offset()

Returns:
Return type:float

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature Offset(offset)

Parameters:offset (float) –

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

PatternType

DurabilityLoadPatternBuilder.PatternType

Returns or sets the pattern type.

-------------------------------------

Getter Method

Signature PatternType()

Returns:
Return type:NXOpen.CAE.DurabilityLoadPatternBuilderPatternTypeEnum

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature PatternType(patternType)

Parameters:patternType (NXOpen.CAE.DurabilityLoadPatternBuilderPatternTypeEnum) –

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Scale

DurabilityLoadPatternBuilder.Scale

Returns or sets the scale.

-------------------------------------

Getter Method

Signature Scale()

Returns:
Return type:float

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature Scale(scale)

Parameters:scale (float) –

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Method Detail

Validate

DurabilityLoadPatternBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.