DurabilityExcitationBuilder Class

class NXOpen.CAE.DurabilityExcitationBuilder

Bases: NXOpen.Builder

Represents the abstract builder class for all durability excitations.

This is an abstract class, and cannot be created.

New in version NX7.5.0.

Properties

Property Description
ExcitationName Returns or sets the excitation name.
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

ExcitationName

DurabilityExcitationBuilder.ExcitationName

Returns or sets the excitation name.

-------------------------------------

Getter Method

Signature ExcitationName()

Returns:
Return type:str

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature ExcitationName(title)

Parameters:title (str) –

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Method Detail

Validate

DurabilityExcitationBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.