LaminateGraphicalReportBuilderSolverInputType Enumeration

NXOpen.CAE.LaminateGraphicalReportBuilder.SolverInputType is an alias for NXOpen.CAE.LaminateGraphicalReportBuilderSolverInputType

class NXOpen.CAE.LaminateGraphicalReportBuilderSolverInputType

Bases: object

Solver input type

Enum Members

Enum Member Enum Member Description
SolverShellStressResultant
Using solver shell stress resultants
SolverPlyStressesAndStrains
Using solver ply stresses
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.