CfdContactPreventionConstraintBuilder Class¶
-
class
NXOpen.CAE.
CfdContactPreventionConstraintBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.CfdContactPreventionConstraint
builderTo create a new instance of this class, use
NXOpen.CAE.CfdContactPreventionConstraintCollection.CreateBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ContactType | Returns or sets the contact type |
FirstSelectElement | Returns the first element selection |
FirstSelection | Returns the first selection |
LocalResolution | Returns the local resolution |
LocalSubdivision | Returns or sets the local subdivision |
NameString | Returns or sets the name string |
PriorityLevel | Returns or sets the priority level |
SecondSelectElement | Returns the second element selection |
SecondSelection | Returns the second selection |
SizingOption | Returns or sets the sizing option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CfdContactPreventionConstraintBuilderContact Enumeration | The contact type. |
CfdContactPreventionConstraintBuilderLocalSubdivisions Enumeration | The local subdivision. |
CfdContactPreventionConstraintBuilderPriority Enumeration | The priority level. |
CfdContactPreventionConstraintBuilderSizing Enumeration | The sizing option. |
Property Detail¶
ContactType¶
-
CfdContactPreventionConstraintBuilder.
ContactType
¶ Returns or sets the contact type
-------------------------------------
Getter Method
Signature
ContactType()
Returns: Return type: NXOpen.CAE.CfdContactPreventionConstraintBuilderContact
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContactType(contactType)
Parameters: contactType ( NXOpen.CAE.CfdContactPreventionConstraintBuilderContact
) –New in version NX11.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
FirstSelectElement¶
-
CfdContactPreventionConstraintBuilder.
FirstSelectElement
¶ Returns the first element selection
-------------------------------------
Getter Method
Signature
FirstSelectElement()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX11.0.0.
License requirements: None.
FirstSelection¶
-
CfdContactPreventionConstraintBuilder.
FirstSelection
¶ Returns the first selection
-------------------------------------
Getter Method
Signature
FirstSelection()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: None.
LocalResolution¶
-
CfdContactPreventionConstraintBuilder.
LocalResolution
¶ Returns the local resolution
-------------------------------------
Getter Method
Signature
LocalResolution()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
LocalSubdivision¶
-
CfdContactPreventionConstraintBuilder.
LocalSubdivision
¶ Returns or sets the local subdivision
-------------------------------------
Getter Method
Signature
LocalSubdivision()
Returns: Return type: NXOpen.CAE.CfdContactPreventionConstraintBuilderLocalSubdivisions
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocalSubdivision(localSubdivision)
Parameters: localSubdivision ( NXOpen.CAE.CfdContactPreventionConstraintBuilderLocalSubdivisions
) –New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
NameString¶
-
CfdContactPreventionConstraintBuilder.
NameString
¶ Returns or sets the name string
-------------------------------------
Getter Method
Signature
NameString()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NameString(nameString)
Parameters: nameString (str) – New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
PriorityLevel¶
-
CfdContactPreventionConstraintBuilder.
PriorityLevel
¶ Returns or sets the priority level
-------------------------------------
Getter Method
Signature
PriorityLevel()
Returns: Return type: NXOpen.CAE.CfdContactPreventionConstraintBuilderPriority
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriorityLevel(priorityLevel)
Parameters: priorityLevel ( NXOpen.CAE.CfdContactPreventionConstraintBuilderPriority
) –New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
SecondSelectElement¶
-
CfdContactPreventionConstraintBuilder.
SecondSelectElement
¶ Returns the second element selection
-------------------------------------
Getter Method
Signature
SecondSelectElement()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX11.0.0.
License requirements: None.
SecondSelection¶
-
CfdContactPreventionConstraintBuilder.
SecondSelection
¶ Returns the second selection
-------------------------------------
Getter Method
Signature
SecondSelection()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: None.
SizingOption¶
-
CfdContactPreventionConstraintBuilder.
SizingOption
¶ Returns or sets the sizing option
-------------------------------------
Getter Method
Signature
SizingOption()
Returns: Return type: NXOpen.CAE.CfdContactPreventionConstraintBuilderSizing
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizingOption(sizingOption)
Parameters: sizingOption ( NXOpen.CAE.CfdContactPreventionConstraintBuilderSizing
) –New in version NX9.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
Method Detail¶
Validate¶
-
CfdContactPreventionConstraintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.