BoltBuilderBoltOperation Enumeration

NXOpen.CAE.BoltBuilder.BoltOperation is an alias for NXOpen.CAE.BoltBuilderBoltOperation

class NXOpen.CAE.BoltBuilderBoltOperation

Bases: object

Represents the options for type of operation

Enum Members

Enum Member Enum Member Description
BoltNut
Creates a bolt connection with nut
BoltTap
Creates a bolt connection in a tapped hole
SpiderJunction
Creates a spider connection at junctions
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.