LaminateZoneType Enumeration¶
NXOpen.CAE.Laminate.ZoneType is an alias for NXOpen.CAE.LaminateZoneType
-
class
NXOpen.CAE.
LaminateZoneType
¶ Bases:
object
Type of zones to export
Enum Members
Enum Member Enum Member Description OrphanElems Zone with elements that were not assigned to any zoneOverlapElems Zone with elements that were assigned to more that one layupRegular Regular valid zoneAll Export all zones-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-