ConstraintResolutionBuilderRule Enumeration

NXOpen.CAE.ConstraintResolutionBuilder.Rule is an alias for NXOpen.CAE.ConstraintResolutionBuilderRule

class NXOpen.CAE.ConstraintResolutionBuilderRule

Bases: object

Constraint Resolution Rule

Enum Members

Enum Member Enum Member Description
ApplyFirstConstraint
apply first constraint on the intersection
ApplySecondConstraint
apply second constraint on the intersection
AverageDofValues
average dof values on the intersection
AddDofValues
add dof values on the intersection
SpecifyDofValues
specify dof values on the intersection
IgnoreConflict
specify dof values on the intersection
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.