ModelUpdateSolutionCollection Class

class NXOpen.CAE.ModelUpdateSolutionCollection

Bases: object

Represents a collection of model update meta solution

To obtain an instance of this class, refer to NXOpen.CAE.CorrelManager

Properties

Property Description
ActiveSolution Returns or sets the active solution

Methods

Method Description
CreateSensitivityViewerBuilder Creates the builder object of model update sensitivity viewer @return
CreateSolutionBuilder Creates the builder object of model update meta solution @return
FindObject Finds a model update meta solution with specified solution name @return Model Update meta solution found

Property Detail

ActiveSolution

ModelUpdateSolutionCollection.ActiveSolution

Returns or sets the active solution

-------------------------------------

Getter Method

Signature ActiveSolution()

Returns:
Return type:NXOpen.CAE.ModelUpdateSolution

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ActiveSolution(activeSolution)

Parameters:activeSolution (NXOpen.CAE.ModelUpdateSolution) –

New in version NX7.5.0.

License requirements: None.

Method Detail

CreateSensitivityViewerBuilder

ModelUpdateSolutionCollection.CreateSensitivityViewerBuilder

Creates the builder object of model update sensitivity viewer

Signature CreateSensitivityViewerBuilder(solution)

Parameters:solution (NXOpen.CAE.ModelUpdateSolution) – Model Update setup
Returns:
Return type:NXOpen.CAE.ModelUpdateSensitivityViewerBuilder

New in version NX7.5.0.

License requirements: nx_correl_update (“FE Model Update”)

CreateSolutionBuilder

ModelUpdateSolutionCollection.CreateSolutionBuilder

Creates the builder object of model update meta solution

Signature CreateSolutionBuilder(solution)

Parameters:solution (NXOpen.CAE.ModelUpdateSolution) – Model update solution being edit
Returns:
Return type:NXOpen.CAE.ModelUpdateSolutionBuilder

New in version NX7.5.0.

License requirements: None.

FindObject

ModelUpdateSolutionCollection.FindObject

Finds a model update meta solution with specified solution name

Signature FindObject(solutionName)

Parameters:solutionName (str) – Solution to be found
Returns:Model Update meta solution found
Return type:NXOpen.CAE.ModelUpdateSolution

New in version NX7.5.0.

License requirements: None.