ElementRevolveBuilderNewMeshType Enumeration

NXOpen.CAE.ElementRevolveBuilder.NewMeshType is an alias for NXOpen.CAE.ElementRevolveBuilderNewMeshType

class NXOpen.CAE.ElementRevolveBuilderNewMeshType

Bases: object

Option to create new mesh or add to existing mesh

Enum Members

Enum Member Enum Member Description
Create
create new mesh
Existing
add to existing mesh
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.