ResultProbeBuilderEdgeIntegral Enumeration¶
NXOpen.CAE.ResultProbeBuilder.EdgeIntegral is an alias for NXOpen.CAE.ResultProbeBuilderEdgeIntegral
-
class
NXOpen.CAE.
ResultProbeBuilderEdgeIntegral
¶ Bases:
object
Options to calculate
CAE.ResultProbeBuilderGeometryValue.WeightedAverage
orCAE.ResultProbeBuilderGeometryValue.Integral
over elements on an edgeEnum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “Length”, ” - ” “Area”, ” - “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.