FEElementLabelMap Class¶
-
class
NXOpen.CAE.
FEElementLabelMap
¶ Bases:
NXOpen.TransientObject
Represents a Elementl Label to an
CAE.FEElement
map, it can be used to quickly convert aCAE.FEElement
label, which is generally used in solver input files and results files, in the element object itselfCAE.FEElement
This is an abstract class
New in version NX6.0.2.
Properties¶
Property | Description |
---|---|
NumElements | Returns the number of CAE.FEElement |
Methods¶
Method | Description |
---|---|
AskElementLabelUsed | Indicates whether input element label is already used or not @return |
AskNextElementLabel | Returns the next CAE.FEElement label from the input put label. |
Dispose | Destroys the object |
GetElement | Returns CAE.FEElement given a CAE.FEElement label @return CAE.FEElement |
Property Detail¶
Method Detail¶
AskElementLabelUsed¶
-
FEElementLabelMap.
AskElementLabelUsed
¶ Indicates whether input element label is already used or not
Signature
AskElementLabelUsed(elementlabel)
Parameters: elementlabel (int) – potential element label Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
AskNextElementLabel¶
-
FEElementLabelMap.
AskNextElementLabel
¶ Returns the next
CAE.FEElement
label from the input put label.Signature
AskNextElementLabel(elementlabel)
Parameters: elementlabel (int) – CAE.FEElement
Label, for first element label input 0Returns: next CAE.FEElement
LabelReturn type: int New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Dispose¶
-
FEElementLabelMap.
Dispose
¶ Destroys the object
Signature
Dispose()
New in version NX6.0.2.
License requirements: None.
GetElement¶
-
FEElementLabelMap.
GetElement
¶ Returns
CAE.FEElement
given aCAE.FEElement
labelSignature
GetElement(elementlabel)
Parameters: elementlabel (int) – CAE.FEElement
LabelReturns: CAE.FEElement
Return type: NXOpen.CAE.FEElement
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)