DestinationCollectorBuilder Class¶
-
class
NXOpen.CAE.
DestinationCollectorBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a Element Collector Container (Ecc) selection
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AutomaticMode | Returns or sets the Automatic Mode value |
ElementContainer | Returns or sets the Element Collector object |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
AutomaticMode¶
-
DestinationCollectorBuilder.
AutomaticMode
¶ Returns or sets the Automatic Mode value
-------------------------------------
Getter Method
Signature
AutomaticMode()
Returns: Return type: bool New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
AutomaticMode(fAutoMode)
Parameters: fAutoMode (bool) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementContainer¶
-
DestinationCollectorBuilder.
ElementContainer
¶ Returns or sets the Element Collector object
-------------------------------------
Getter Method
Signature
ElementContainer()
Returns: Return type: NXOpen.CAE.MeshCollector
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
ElementContainer(pElementContainer)
Parameters: pElementContainer ( NXOpen.CAE.MeshCollector
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)