ModelUpdateCorrelMethodBuilderMethod Enumeration

NXOpen.CAE.ModelUpdateCorrelMethodBuilder.Method is an alias for NXOpen.CAE.ModelUpdateCorrelMethodBuilderMethod

class NXOpen.CAE.ModelUpdateCorrelMethodBuilderMethod

Bases: object

correlation method option

Enum Members

Enum Member Enum Member Description
Mac
Correlation Method is MAC
XOrtho
Correlation Method is X_ORTHO
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.