SimSimulationObjectGroup Class¶
-
class
NXOpen.CAE.
SimSimulationObjectGroup
¶ Bases:
NXOpen.CAE.SimBcGroup
Represents a simulation object group in a solution or solution step
Not support KF.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
GroupContainer | Returns the solution or solution step owning this BC group |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Add | Adds a simulation object to this group |
GetSimulationObjects | Gets the simulation objects in this group @return the simulation objects in this group |
Remove | Removes a simulation object from this group |
RemoveAll | Removes all simulation objects from this group |
SetBoltLoadSequence | Set the bolt load sequence |
Method Detail¶
Add¶
-
SimSimulationObjectGroup.
Add
¶ Adds a simulation object to this group
Signature
Add(tSimulationObject)
Parameters: tSimulationObject ( NXOpen.CAE.SimSimulationObject
) – the simulation object to be addedNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetSimulationObjects¶
-
SimSimulationObjectGroup.
GetSimulationObjects
¶ Gets the simulation objects in this group
Signature
GetSimulationObjects()
Returns: the simulation objects in this group Return type: list of NXOpen.CAE.SimSimulationObject
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Remove¶
-
SimSimulationObjectGroup.
Remove
¶ Removes a simulation object from this group
Signature
Remove(pSimulationObject)
Parameters: pSimulationObject ( NXOpen.CAE.SimSimulationObject
) – the simulation object to be removedNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)