AfuMathOperationOutputType Enumeration

NXOpen.CAE.AfuMathOperation.OutputType is an alias for NXOpen.CAE.AfuMathOperationOutputType

class NXOpen.CAE.AfuMathOperationOutputType

Bases: object

Defines the output type of new AFU Data Record

Enum Members

Enum Member Enum Member Description
Append
Appends the new AFU Data Record to the source AFU file
Overwrite
Overwrites the source AFU Data Record
OtherFile
Saves the new AFU Data Record to other file
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.