CAEWeldConnectionBuilderWeldTypeEnum Enumeration

NXOpen.CAE.CAEWeldConnectionBuilder.WeldTypeEnum is an alias for NXOpen.CAE.CAEWeldConnectionBuilderWeldTypeEnum

class NXOpen.CAE.CAEWeldConnectionBuilderWeldTypeEnum

Bases: object

the type of weld connection to be created

Enum Members

Enum Member Enum Member Description
PointToPointDirect
It’s a point to point direct weldconnection,mesh points are created during weld connection
PointToPointIndirect
It’s a point to point in-direct weldconnection,RBE3 elements are created during weld connection
PointToPoint3dWeld
It’s a point to point in-direct weldconnection,3D elements are created during weld connection
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.