DurabilityStressAxesBuilderElementFaceStressAxisEnum Enumeration

NXOpen.CAE.DurabilityStressAxesBuilder.ElementFaceStressAxisEnum is an alias for NXOpen.CAE.DurabilityStressAxesBuilderElementFaceStressAxisEnum

class NXOpen.CAE.DurabilityStressAxesBuilderElementFaceStressAxisEnum

Bases: object

the Element Face Stress Axis Enum.

Enum Members

Enum Member Enum Member Description
BiAxial
BiAxial
UniAxial
UniAxial
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.