DurabilityEventOverridesBuilderUseElementsEnum Enumeration

NXOpen.CAE.DurabilityEventOverridesBuilder.UseElementsEnum is an alias for NXOpen.CAE.DurabilityEventOverridesBuilderUseElementsEnum

class NXOpen.CAE.DurabilityEventOverridesBuilderUseElementsEnum

Bases: object

the use elements enum.

Enum Members

Enum Member Enum Member Description
All
All
Select
Select
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.