PolygonGeometryManager Class¶
-
class
NXOpen.CAE.
PolygonGeometryManager
¶ Bases:
object
Provides methods for managing set
NXOpen.CAE.PolygonGeometryManager
Use the
NXOpen.CAE.GeometryRecipeCollection
class to create a recipe.New in version NX10.0.0.
“CaeGeometryRecipes”, ” Returns the geometry recipes belonging to the FEM. “
Methods¶
Method | Description |
---|---|
GetPolygonBodyResolutionOnFemBodies | Gets the tesselation on polygon bodies that were created from CAD bodies. |
SetPolygonBodyResolutionOnFemBodies | Sets the tesselation on polygon bodies that were created from CAD bodies. |
SetPolygonBodyResolutionWithRecreate | Set Resolution for polygon body with recreate body only @return |
SetPolygonBodyResolutionWithRecreateAndUpdate | Set Resolution for polygon body with recreate body and update only @return |
Enumerations¶
PolygonGeometryManagerPolygonBodyResolutionType Enumeration | Entity type |
CaeGeometryRecipes¶
-
PolygonGeometryManager.
CaeGeometryRecipes
¶ Returns the geometry recipes belonging to the FEM.
Signature
CaeGeometryRecipes()
New in version NX10.0.0.
Returns: Return type: NXOpen.CAE.GeometryRecipeCollection
Method Detail¶
GetPolygonBodyResolutionOnFemBodies¶
-
PolygonGeometryManager.
GetPolygonBodyResolutionOnFemBodies
¶ Gets the tesselation on polygon bodies that were created from CAD bodies.
Signature
GetPolygonBodyResolutionOnFemBodies()
Returns: Tesselation on all polygon bodies Return type: NXOpen.CAE.PolygonGeometryManagerPolygonBodyResolutionType
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetPolygonBodyResolutionOnFemBodies¶
-
PolygonGeometryManager.
SetPolygonBodyResolutionOnFemBodies
¶ Sets the tesselation on polygon bodies that were created from CAD bodies.
Signature
SetPolygonBodyResolutionOnFemBodies(resType)
Parameters: resType ( NXOpen.CAE.PolygonGeometryManagerPolygonBodyResolutionType
) – Tesselation on all polygon bodiesNew in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetPolygonBodyResolutionWithRecreate¶
-
PolygonGeometryManager.
SetPolygonBodyResolutionWithRecreate
¶ Set Resolution for polygon body with recreate body only
Signature
SetPolygonBodyResolutionWithRecreate(resolutionType, inPolygonBodies)
Parameters: - resolutionType (
NXOpen.CAE.PolygonGeometryManagerPolygonBodyResolutionType
) – - inPolygonBodies (list of
NXOpen.CAE.CAEBody
) –
Returns: Return type: list of
NXOpen.CAE.CAEBody
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- resolutionType (
SetPolygonBodyResolutionWithRecreateAndUpdate¶
-
PolygonGeometryManager.
SetPolygonBodyResolutionWithRecreateAndUpdate
¶ Set Resolution for polygon body with recreate body and update only
Signature
SetPolygonBodyResolutionWithRecreateAndUpdate(resolutionType, inPolygonBodies)
Parameters: - resolutionType (
NXOpen.CAE.PolygonGeometryManagerPolygonBodyResolutionType
) – - inPolygonBodies (list of
NXOpen.CAE.CAEBody
) –
Returns: Return type: list of
NXOpen.CAE.CAEBody
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- resolutionType (