BoltBuilderSelection Enumeration¶
NXOpen.CAE.BoltBuilder.Selection is an alias for NXOpen.CAE.BoltBuilderSelection
-
class
NXOpen.CAE.
BoltBuilderSelection
¶ Bases:
object
Represents the options for entity selection
Enum Members
Enum Member Enum Member Description Edge Allows edge selection for head/nut/junctionPoint Allows point selection for head/nut/junction-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-