SliverFaceMethod Class

class NXOpen.CAE.SliverFaceMethod

Bases: NXOpen.SelectionMethod

Represents the output from the sliver face smart selector method

To obtain an instance of this class use CAE::SmartSelectionManager

New in version NX6.0.0.

Methods

Method Description
Dispose Frees the object from memory.
GetFaces Returns the resultant faces @return Resultant faces
GetSelectedObjects Returns the objects selected by this NXOpen.SelectionMethod.

Method Detail

Dispose

SliverFaceMethod.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX6.0.0.

License requirements: None.

GetFaces

SliverFaceMethod.GetFaces

Returns the resultant faces

Signature GetFaces()

Returns:Resultant faces
Return type:list of NXOpen.CAE.CAEFace

New in version NX6.0.4.

License requirements: None.