DurabilityEventFatigueSettingsBuilderFatigueSafetyFactorMethodEnum Enumeration

NXOpen.CAE.DurabilityEventFatigueSettingsBuilder.FatigueSafetyFactorMethodEnum is an alias for NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueSafetyFactorMethodEnum

class NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueSafetyFactorMethodEnum

Bases: object

the Fatigue Safety Factor Method Enum.

Enum Members

Enum Member Enum Member Description
AmplitudeandMean
AmplitudeandMean
Amplitude
Amplitude
Mean
Mean
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.