ElementTypeBuilderElementOrderType Enumeration

NXOpen.CAE.ElementTypeBuilder.ElementOrderType is an alias for NXOpen.CAE.ElementTypeBuilderElementOrderType

class NXOpen.CAE.ElementTypeBuilderElementOrderType

Bases: object

Order of the element types to be specified.

Enum Members

Enum Member Enum Member Description
Any
any element
Linear
linear element
Parabolic
parabolic element
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.