SpringEADBuilderState Enumeration¶
NXOpen.CAE.SpringEADBuilder.State is an alias for NXOpen.CAE.SpringEADBuilderState
-
class
NXOpen.CAE.
SpringEADBuilderState
¶ Bases:
object
indicates to apply or clear the stiffness property upon commit
Enum Members
Enum Member Enum Member Description Apply apply the propertyClear clear the property-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-