SurfaceCoatBuilderSelectionMethod Enumeration

NXOpen.CAE.SurfaceCoatBuilder.SelectionMethod is an alias for NXOpen.CAE.SurfaceCoatBuilderSelectionMethod

class NXOpen.CAE.SurfaceCoatBuilderSelectionMethod

Bases: object

Represents the selection method to be used

Enum Members

Enum Member Enum Member Description
ThreeDimensionMesh
3D mesh
ElementFreeFace
Element free faces
Geometry
Face or body
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.