SimLoadSet Class¶
-
class
NXOpen.CAE.
SimLoadSet
¶ Bases:
NXOpen.CAE.NamedPropertyTable
,NXOpen.CAE.IExportableFEEntity
Represents a cae load set object
To create a new instance of this class, use
NXOpen.CAE.SimLoadSetCollection.CreateLoadSet()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DescriptorName | Returns the name of the load set descriptor |
DescriptorType | Returns the descriptor name defines the type of the property table in named property table holder |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Label | Returns or sets the label of the named property table holder |
LanguageName | Returns the lanugage of the descriptor that defines the type of the property table in named property table holder |
LoadSetType | Returns the type of the load set |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PropertyTable | Returns the property table of the named property table holder |
Prototype | Returns the prototype of this object if it is an occurrence. |
SolverName | Returns the solver of lanugage of the descriptor that defines the type of the property table in named property table holder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddMemberFolders | Add root folder members to load set. |
AddMemberLoads | Add load members to load set. |
AddMemberSet | Add a load set member to load set. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMemberFolderValidLoads | Get all valid loads under given root folder in given load set |
GetMemberFolders | Get all root folder memebers of load set |
GetMemberLoads | Get all load memebers from load set |
GetMemberSet | Get the load set memeber from load set @return member load set |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSolverCardSyntax | Returns the solver card syntax strings for this entity. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
RemoveMemberFolders | Remove root folder memebers from load set |
RemoveMemberLoads | Remove load memebers from load set |
RemoveMemberSet | Remove a load set memeber from load set |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
SimLoadSetType Enumeration | Load Set type |
Property Detail¶
DescriptorName¶
-
SimLoadSet.
DescriptorName
¶ Returns the name of the load set descriptor
-------------------------------------
Getter Method
Signature
DescriptorName()
Returns: Return type: str New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsOccurrence¶
-
SimLoadSet.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SimLoadSet.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
LoadSetType¶
-
SimLoadSet.
LoadSetType
¶ Returns the type of the load set
-------------------------------------
Getter Method
Signature
LoadSetType()
Returns: Return type: NXOpen.CAE.SimLoadSetType
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Name¶
-
SimLoadSet.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SimLoadSet.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SimLoadSet.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SimLoadSet.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddMemberFolders¶
-
SimLoadSet.
AddMemberFolders
¶ Add root folder members to load set.
Only load set with type of
SimLoadSetType.Static
andSimLoadSetType.Acoustic
andSimLoadSetType.Temperature
can add member folderSignature
AddMemberFolders(tmembers)
Parameters: tmembers (list of NXOpen.CAE.SimLbcFolder
) – member foldersNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AddMemberLoads¶
-
SimLoadSet.
AddMemberLoads
¶ Add load members to load set.
Only load set with type of
SimLoadSetType.Static
andSimLoadSetType.Acoustic
andSimLoadSetType.Temperature
can add member loadSignature
AddMemberLoads(tmembers)
Parameters: tmembers (list of NXOpen.CAE.SimLoad
) – member loadsNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AddMemberSet¶
-
SimLoadSet.
AddMemberSet
¶ Add a load set member to load set.
Only load set with type of
SimLoadSetType.Frequency
andSimLoadSetType.Transient
can add only one set member with type ofSimLoadSetType.Static
Signature
AddMemberSet(tmember)
Parameters: tmember ( NXOpen.CAE.SimLoadSet
) – member load setNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
SimLoadSet.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetMemberFolderValidLoads¶
-
SimLoadSet.
GetMemberFolderValidLoads
¶ Get all valid loads under given root folder in given load set
Signature
GetMemberFolderValidLoads(tFolder)
Parameters: tFolder ( NXOpen.CAE.SimLbcFolder
) – member folderReturns: member loads under folder Return type: list of NXOpen.CAE.SimLoad
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetMemberFolders¶
-
SimLoadSet.
GetMemberFolders
¶ Get all root folder memebers of load set
Signature
GetMemberFolders()
Returns: member folders Return type: list of NXOpen.CAE.SimLbcFolder
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetMemberLoads¶
-
SimLoadSet.
GetMemberLoads
¶ Get all load memebers from load set
Signature
GetMemberLoads()
Returns: member loads Return type: list of NXOpen.CAE.SimLoad
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetMemberSet¶
-
SimLoadSet.
GetMemberSet
¶ Get the load set memeber from load set
Signature
GetMemberSet()
Returns: member load set Return type: NXOpen.CAE.SimLoadSet
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetSolverCardSyntax¶
-
SimLoadSet.
GetSolverCardSyntax
¶ Returns the solver card syntax strings for this entity.
Signature
GetSolverCardSyntax()
Returns: Return type: list of str New in version NX8.5.0.
License requirements: None.
Print¶
-
SimLoadSet.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveMemberFolders¶
-
SimLoadSet.
RemoveMemberFolders
¶ Remove root folder memebers from load set
Signature
RemoveMemberFolders(tmembers)
Parameters: tmembers (list of NXOpen.CAE.SimLbcFolder
) – member foldersNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveMemberLoads¶
-
SimLoadSet.
RemoveMemberLoads
¶ Remove load memebers from load set
Signature
RemoveMemberLoads(tmembers)
Parameters: tmembers (list of NXOpen.CAE.SimLoad
) – member loadsNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveMemberSet¶
-
SimLoadSet.
RemoveMemberSet
¶ Remove a load set memeber from load set
Signature
RemoveMemberSet(tmember)
Parameters: tmember ( NXOpen.CAE.SimLoadSet
) – member load setNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetName¶
-
SimLoadSet.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.