SimLoadSetType Enumeration¶
NXOpen.CAE.SimLoadSet.Type is an alias for NXOpen.CAE.SimLoadSetType
-
class
NXOpen.CAE.
SimLoadSetType
¶ Bases:
object
Load Set type
Enum Members
Enum Member Enum Member Description Invalid Static load set.Static Static load set.Frequency Frequency Excitation Load Set.Transient Transient Excitation Load Set.Acoustic Acoustic Source Load Set.Temperature Temperature Set.Bolt Bolt Load Set.InitialStressStrain Initial Stress/Strain Load Set-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-