NodeElementInfoManager Class¶
-
class
NXOpen.CAE.
NodeElementInfoManager
¶ Bases:
object
Provides method for creating builder for node element info operation commands in both sim and fem part
To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateAssignNodalCsBuilder | Creates a builder for assigning nodal cs @return |
CreateNodeElementInfoBuilder | Creates a builder for node element info command @return |
CreateThicknessBuilder | Creates a builder for node element info command @return |
CreateThicknessPlotContoursBuilder | Creates a builder for plotting thickness contours @return |
Method Detail¶
CreateAssignNodalCsBuilder¶
-
NodeElementInfoManager.
CreateAssignNodalCsBuilder
¶ Creates a builder for assigning nodal cs
Signature
CreateAssignNodalCsBuilder()
Returns: Return type: NXOpen.CAE.AssignNodalCSBuilder
New in version NX7.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeElementInfoBuilder¶
-
NodeElementInfoManager.
CreateNodeElementInfoBuilder
¶ Creates a builder for node element info command
Signature
CreateNodeElementInfoBuilder()
Returns: Return type: NXOpen.CAE.NodeElementInfoBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateThicknessBuilder¶
-
NodeElementInfoManager.
CreateThicknessBuilder
¶ Creates a builder for node element info command
Signature
CreateThicknessBuilder(meshContext)
Parameters: meshContext ( NXOpen.CAE.Mesh
) – Mesh object for thickness data accessReturns: Return type: NXOpen.CAE.ThicknessBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateThicknessPlotContoursBuilder¶
-
NodeElementInfoManager.
CreateThicknessPlotContoursBuilder
¶ Creates a builder for plotting thickness contours
Signature
CreateThicknessPlotContoursBuilder()
Returns: Return type: NXOpen.CAE.ThicknessPlotContoursBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)