CaePart Class¶
-
class
NXOpen.CAE.
CaePart
¶ Bases:
NXOpen.BasePart
This is an abstract class for NX parts of type .fem and .sim
This is an abstract class
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ComponentAssembly | Returns the component assembly. |
FieldManager | Returns the field main. |
FullPath | Returns the full path of the part. |
HasWriteAccess | Returns the write-access status of a part independent of the load state. |
IsFullyLoaded | Returns the load status of a part. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsReadOnly | Returns the read-only status of a part. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Leaf | Returns the leaf name of the part. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PartPreviewMode | Returns or sets the preview mode |
PartUnits | Returns the units of the part file. |
Prototype | Returns the prototype of this object if it is an occurrence. |
SaveDisplayFacets | Returns or sets whether display quality facets are saved in the part file |
Tag | Returns the Tag for this object. |
UniqueIdentifier | Returns or sets the unique identifier for this part used to determine whether parts can be quietly substituted during part open. |
PhysicalPropertyTables |
|
ModelingObjectPropertyTables |
|
CaeGroups |
|
SmartSelectionMgr |
|
NodeElementInfoMgr |
|
SelectElementMgr |
|
MeshControlDisplayMgr |
|
ModelCheckMgr |
|
ShowHideMgr |
|
ElementQualitySettings |
|
CaeQueryCurves |
|
LayoutStates |
|
PostScenarioMgr |
|
BoundingVolumes |
|
Methods¶
Method | Description |
---|---|
AssignPermanentName | Saves a temporary part with the given name. |
CanBeDisplayPart | Returns true if the part can be displayed and false if not displayed @return |
Close | Closes an open part. |
CompleteStructure | Make additions necessary to complete the incomplete assembly structure of the input part |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
CreateDynamicSectionBuilder | Creates a NXOpen.Display.DynamicSectionBuilder The base part must be a displayable part, otherwise an exception will be thrown. |
CreateEffectivityConditionBuilder | Creates a NXOpen.EffectivityConditionBuilder @return |
CreateFacetSettingsBuilder | Creates a builder for the Facet Settings dialog @return |
CreateGatewayGroupBuilder | Creates a Groups builder @return GroupBuilder object |
CreateModelDisplayBuilder | Creates a builder for model display controls command @return |
CreatePerspectiveOptionsBuilder | Creates a builder for the Perspective Options dialog @return |
CreateReferenceSet | Creates a NXOpen.ReferenceSet object @return New reference set object |
CreateSolverAppendOption | Returns a solver append option object for importing the solver specific data into an existing NXOpen.CAE.FemPart or NXOpen.CAE.SimPart . |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteReferenceSet | Deletes a NXOpen.ReferenceSet object |
DeleteSolverAppendOption | Deletes a solver append option object for importing the solver specific data into an existing NXOpen.CAE.FemPart or NXOpen.CAE.SimPart . |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
ExportJt | Exports JT file |
ExportSimulation | Exports the Simulation data for a NXOpen.CAE.CaePart . |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAllReferenceSets | Get all the NXOpen.ReferenceSet objects in this part. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCollaborativeContentType | The collaborative content type of this part. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetCsysFlattenedLabel | Gets the resolved label of csys in cae part. |
GetDescription | Gets the description assoicated with the Cae part |
GetHistoryInformation | Get history of part @return list of history data for the part. |
GetIncompleteStatus | Inquire whether the provided part is flagged as being incomplete @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMakeUniqueName | Gets the Unique name on a part for the Make Unique operation @return |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPreviewImage | Get the preview image This will return the graphic preview image of the part (when available). |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetTransientStatus | Inquire whether the provided part is flagged as being transient @return |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
ImportExistingSimulation | Imports the solver specific data into an existing NXOpen.CAE.FemPart or NXOpen.CAE.SimPart . |
LoadFeatureDataForSelection | Ensure that feature data is loaded for a part. |
LoadFully | Ensures that this part is fully loaded. |
LoadThisPartFully | Ensures that this part is fully loaded. |
NewBeamSectionOffsetOptions | Creates a NXOpen.CAE.BeamSectionOffsetOptions @return |
NewBeamSectionOptions | Creates a NXOpen.CAE.BeamSectionOptions @return the syncrhonize options object created |
NewBeamSectionOrientationOptions | Creates a NXOpen.CAE.BeamSectionOrientationOptions @return |
NewMaterialOptions | Creates a NXOpen.CAE.MaterialOptions @return the material options object created |
Prints a representation of this object to the system log file. | |
RegenerateDisplayFacets | Regenerates display specific transient cached facets in the part. |
ReinstateTransience | Reinstate the transient status to the formerly transient input part |
RemoveTransience | Remove the transient status from the input part |
Reopen | Reopens a loaded part. |
ReopenAs | Reopens a loaded part. |
ReverseBlankAll | Reverse blank all the objects in the part. |
Save | Saves the part whether it is modified or not. |
SaveAs | Creates copy of target part. |
SaveBookmark | Saves a bookmark file. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDescription | Sets the description assoicated with the Cae part |
SetMakeUniqueName | Sets the unique name on part for the Make Unique operation |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
CaePart.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CaePart.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
CaePart.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CaePart.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CaePart.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
CaePart.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
PhysicalPropertyTables¶
-
CaePart.
PhysicalPropertyTables
¶ Returns the physical property table collection belonging to this CAE Part
Signature
PhysicalPropertyTables()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.PhysicalPropertyTableCollection
ModelingObjectPropertyTables¶
-
CaePart.
ModelingObjectPropertyTables
¶ Returns the modeling object property table collection belonging to this CAE Part
Signature
ModelingObjectPropertyTables()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.ModelingObjectPropertyTableCollection
CaeGroups¶
-
CaePart.
CaeGroups
¶ Returns the CAE Group collection belonging to this Part
Signature
CaeGroups()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.CaeGroupCollection
SmartSelectionMgr¶
-
CaePart.
SmartSelectionMgr
¶ Returns the smart selection manager belonging to this part
Signature
SmartSelectionMgr()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.SmartSelectionManager
NodeElementInfoMgr¶
-
CaePart.
NodeElementInfoMgr
¶ Returns the node element info manager belonging to this IFem
Signature
NodeElementInfoMgr()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.NodeElementInfoManager
SelectElementMgr¶
-
CaePart.
SelectElementMgr
¶ Returns the select element manager belonging to this IFem
Signature
SelectElementMgr()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.SelectElementsManager
MeshControlDisplayMgr¶
-
CaePart.
MeshControlDisplayMgr
¶ Returns the mesh control display manager belonging to this IFem
Signature
MeshControlDisplayMgr()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.MeshControlDisplayManager
ModelCheckMgr¶
-
CaePart.
ModelCheckMgr
¶ Returns the select element manager belonging to this IFem
Signature
ModelCheckMgr()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.ModelCheckManager
ShowHideMgr¶
-
CaePart.
ShowHideMgr
¶ Returns the show hide manager belonging to the part
Signature
ShowHideMgr()
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.ShowHideManager
ElementQualitySettings¶
-
CaePart.
ElementQualitySettings
¶ Returns the element quality settings collection belonging to this CAE Part
Signature
ElementQualitySettings()
New in version NX8.5.0.
Returns: Return type: NXOpen.CAE.ModelCheck.ElementQualitySettingCollection
CaeQueryCurves¶
-
CaePart.
CaeQueryCurves
¶ Returns the CAE query curve manager belonging to this Part
Signature
CaeQueryCurves()
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.QueryCurveManager
LayoutStates¶
-
CaePart.
LayoutStates
¶ Contains a
NXOpen.CAE.LayoutStateCollection
.Signature
LayoutStates()
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.LayoutStateCollection
PostScenarioMgr¶
-
CaePart.
PostScenarioMgr
¶ Contains a
NXOpen.CAE.PostScenarioManager
.Signature
PostScenarioMgr()
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.PostScenarioManager
BoundingVolumes¶
-
CaePart.
BoundingVolumes
¶ Contains a
NXOpen.CAE.BoundingVolumeCollection
.Signature
BoundingVolumes()
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.BoundingVolumeCollection
Method Detail¶
CreateModelDisplayBuilder¶
-
CaePart.
CreateModelDisplayBuilder
¶ Creates a builder for model display controls command
Signature
CreateModelDisplayBuilder()
Returns: Return type: NXOpen.CAE.ModelDisplayBuilder
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateSolverAppendOption¶
-
CaePart.
CreateSolverAppendOption
¶ Returns a solver append option object for importing the solver specific data into an existing
NXOpen.CAE.FemPart
orNXOpen.CAE.SimPart
.Signature
CreateSolverAppendOption()
Returns: the object of solver append option Return type: NXOpen.CAE.SolverAppendOption
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteSolverAppendOption¶
-
CaePart.
DeleteSolverAppendOption
¶ Deletes a solver append option object for importing the solver specific data into an existing
NXOpen.CAE.FemPart
orNXOpen.CAE.SimPart
.Signature
DeleteSolverAppendOption(appendOption)
Parameters: appendOption ( NXOpen.CAE.SolverAppendOption
) – the object of solver append optionNew in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ExportJt¶
-
CaePart.
ExportJt
¶ Exports JT file
Signature
ExportJt(fileName)
Parameters: fileName (str) – the JT file name to be created New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ExportSimulation¶
-
CaePart.
ExportSimulation
¶ Exports the Simulation data for a
NXOpen.CAE.CaePart
.For a
NXOpen.CAE.SimPart
, the data will be exported for the active solutionNXOpen.CAE.SimSolution
if its solver matches the specified solverName.For a
NXOpen.CAE.FemPart
, the data will be exported only if the solver defined for theNXOpen.CAE.FemPart
matches the specified solverName.Export is driven by the properties defined in the input
NXOpen.CAE.CaeDataContainer
propertyList. The exact properties can vary from solver to solver. An accurate list of property names is obtained by journaling the opertation first.Signature
ExportSimulation(solverName, propertyList)
Parameters: - solverName (str) – the name of the solver export
- propertyList (
NXOpen.CAE.CaeDataContainer
) – the export parameters. SeeCAE.CaeSession.GetDataContainer()
.
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
CaePart.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetCsysFlattenedLabel¶
-
CaePart.
GetCsysFlattenedLabel
¶ Gets the resolved label of csys in cae part.
Signature
GetCsysFlattenedLabel(csys)
Parameters: csys ( NXOpen.CoordinateSystem
) – coordinate systemReturns: resolved label Return type: int New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetDescription¶
-
CaePart.
GetDescription
¶ Gets the description assoicated with the Cae part
Signature
GetDescription()
Returns: description Return type: list of str New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ImportExistingSimulation¶
-
CaePart.
ImportExistingSimulation
¶ Imports the solver specific data into an existing
NXOpen.CAE.FemPart
orNXOpen.CAE.SimPart
.The data will be imported only if the solver defined for the
NXOpen.CAE.FemPart
orNXOpen.CAE.SimPart
matches the specified solverName.Import is driven by the properties defined in the input
NXOpen.CAE.CaeDataContainer
propertyList. The exact properties can vary from solver to solver. An accurate list of property names is obtained by journaling the opertation first.Signature
ImportExistingSimulation(solverName, propertyList)
Parameters: - solverName (str) – the name of the solver import
- propertyList (
NXOpen.CAE.CaeDataContainer
) – the import parameters. SeeCAE.CaeSession.GetDataContainer()
.
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
NewBeamSectionOffsetOptions¶
-
CaePart.
NewBeamSectionOffsetOptions
¶ Creates a
NXOpen.CAE.BeamSectionOffsetOptions
Signature
NewBeamSectionOffsetOptions()
Returns: Return type: NXOpen.CAE.BeamSectionOffsetOptions
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NewBeamSectionOptions¶
-
CaePart.
NewBeamSectionOptions
¶ Creates a
NXOpen.CAE.BeamSectionOptions
Signature
NewBeamSectionOptions()
Returns: the syncrhonize options object created Return type: NXOpen.CAE.BeamSectionOptions
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NewBeamSectionOrientationOptions¶
-
CaePart.
NewBeamSectionOrientationOptions
¶ Creates a
NXOpen.CAE.BeamSectionOrientationOptions
Signature
NewBeamSectionOrientationOptions()
Returns: Return type: NXOpen.CAE.BeamSectionOrientationOptions
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NewMaterialOptions¶
-
CaePart.
NewMaterialOptions
¶ Creates a
NXOpen.CAE.MaterialOptions
Signature
NewMaterialOptions()
Returns: the material options object created Return type: NXOpen.CAE.MaterialOptions
New in version NX5.0.0.
License requirements: None.
Print¶
-
CaePart.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetDescription¶
-
CaePart.
SetDescription
¶ Sets the description assoicated with the Cae part
Signature
SetDescription(description)
Parameters: description (list of str) – description New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetName¶
-
CaePart.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.